Jump to content
OMRON Forums

sushant.dighe

Members
  • Posts

    4
  • Joined

  • Last visited

Everything posted by sushant.dighe

  1. I have fresh power PMAC controller 1.when i'm start first time motor(#1j+/#1j-) is working fine. 2.when i use some unwanted command on motor that time PWR LED is off and motor not working . And error showing Motor not active ( then i check in troubleshooting why motor is not running there shows motor[x].ServoCtrl is wrong value set but these value set automatically then i correct this error and once again write the command #1j+/#1j- that time i get the motor[x].FeFatal error how to resolve this issue ? 3.now i need to how to run motor continues ? 4.see below program // &1 // Address C.S. 1 // #1->1000X // Motor 1 assigned to X-axis, 1000 counts/unit // Motion program code open prog 1 // Open buffer for entry linear; // Linear interpolation move mode abs; // Absolute move mode ta500; // 1/2-second accel/decel time ts0; // No S-curve accel/decel time f5; // Speed of 5 axis units per time unit X10; // Move X-axis to position of 10 units dwell500; // Sit here for 1/2-second X0; // Move X-axis to position of 0 units dwell500; // Sit here for 1/2-second close // Close buffer, end program entry how to run above motion program code
×
×
  • Create New...