Turbo PMAC2, Geo Direct PWM, PEWin 32.
I have gone thru the motor/drive setup and tuning using the utility in PEWin32 for a single axis. At the end, it had an option for copying the set-up to a second motor/axis. I wanted to test the first setup a little and did that and it is running properly. For the life of me, I cannot find a way to simply copy the same setup parameters at once to the second identical axis/drive channel.
Other than going thru the iX00..99 one at a time and transferring the values to the next axis, is there a convenient way to do this?
I even tried stepping thru the setup utility again but it doesn't want to let me step thru all the steps without re-doing some of the tests.
Thanks,
CDN