orhirshfeld
Members-
Posts
18 -
Joined
-
Last visited
orhirshfeld's Achievements
-
This list was last updated 3 years ago in 2017 I wonder if you have any updates Thanks Or Hirshfeld SW Control Engineer FFRobotics https://www.linkedin.com/in/orhirshfeld/
-
We have NY-51 Controller with Linux Ubuntu installed We have some issues with our EtherCAT communication and we wish to diagnose it. But we are suffering many crashes when we are using Diagnosis mode in EtherCAT. We tried the IDE on different PC but got the same results it's very frustrating and hard to diagnose the problem We are using IDE version 4.1.0.25 did you encounter a similar problem? is there a way to slove it? Can we use EC-Enginner by Acontis to diagnose the communication?
-
Can I install PowerPMAC IDE Patch Release (Version 4.2.1.19) if I have 4.1.0.24 already installed? What are the changes made in this version?
-
Does PPMAC EtherCAT Master supports Modular Devices?
orhirshfeld replied to kjcho's topic in Power PMAC
Is still not supported? I'm using Power Pmac IDE version 4.1.0.24 with PPMAC NY-51 Controller (CPU:X86 Firmware:2.5.0.0) I wish to connect to FESTO CTEU and they provide few different ESI I'm not sure which one I should load, also the ESI Manager doesn't let load all files, I believe because there are two files with the same name. They give two types, one suitable for OMRON Sysmac Studio and other type is for suitable for BECKHOFF TwinCAT readme file of FESTO: Festo CTEU-EtherCAT ESI files Default behaviour of our CTEU-EC is Modular Device Profile (MDP). To change it please take a look on "CTEU-EC Config fix-mdp_EN.pdf" for reprogramming the EEPROM. In this package you find following ESI files for OMROM Sysmac Studio and Beckhoff TwinCAT: OMROM Festo CTEU-EtherCAT Modular - use it if PLC support MDP (work Sysmac Studio > V1.06) Festo CTEU-EtherCAT Fix - can be used after reprogramming the EEPROM on most PLCs TwinCAT Festo CTEU-EtherCAT Modular - use it if PLC support MDP Festo CTEU-EtherCAT Fix - USINT - can be used after reprogramming the EEPROM on all PLCs Festo CTEU-EtherCAT Fix - BYTEARR - can be used after reprogramming the EEPROM on most PLCs Please install only one Fix configuration ESI files at the same time. -
I encountered a similar issue and I got an error from IDE also, I succeed to connect with ssh but when I try to run "gpascii" or "sendgetsends" i get the following error: rtpmac open, Err Msg: (No such device or address) Segmentation fault I attached photos to this post to demonstrate to errors I got I wonder if you encountered a similar issue to what I described in this post? also I saw that there are two versions of MotionCore.zip files on the fieldepot: MotionCore.zip old version: ftp://ftp.deltatau.ch/Virtual-PowerPMAC-pack/OLD/MotionCore.zip MotionCore.zip latest version ftp://ftp.deltatau.ch/Virtual-PowerPMAC-pack/MotionCore.zip I tried both and failed, did you tried both? Host OS : Ubuntu 16.04 VM SW: VirtualBox 6.0.6 IDE 4.1.0.24 running on Virtual Machine of Win10 Thank you, Or Hirshfeld SW Control Engineer FFRobotics https://www.linkedin.com/in/orhirshfeld/
-
Switching between Linear to Rapid Mode cause EtherCAT failure
orhirshfeld replied to orhirshfeld's topic in Power PMAC
the motor status shows AmpFault The AmpFault indicate error source in Motor (pAmpFault=ECAT[0].IO[4127].Data.a) Axor motor error code indicating Error in getting SYNC msgs ECAT[0].MasterState=8 (OP) "ecat slaves" return all OP mode Motor Conversion = 2184.53 pulses/mm RapidSpeedSel=0 MaxSpeed=3276.7949 (1.5 m/s) in 1st fast movement and 218.453 (0.1 m/s) in 2nd slow movement. JogSpeed=3276.7949 (1.5 m/s) JogTa=-0.030517625 (15 m/s^2) JogTs=0 The motor is running at Rated Speed, 3000 RPM (1.5 m/s) We measured torque and found that motor only using below 20% of rated torque at worst case. Triggered moves can be homing, jogging or rapid from in program. -
Switching between Linear to Rapid Mode cause EtherCAT failure
orhirshfeld replied to orhirshfeld's topic in Power PMAC
Motor Status Window show AmpFault and Axor Motor return a manufacturer specific EtherCAT error code, the error indicates that it didn't get SYNC msgs for 3ms according to Axor Support. in "ecat slaves" all stay in Operational (OP) EtherCAT Mode Triggered moves can be homing, jogging or rapid from in program. -
We have MotionCore IPC connected to Axor motors using EtherCAT the movement of the motors is split into three parts, the first part is moving fast according to the required profile, the second part is to move slow and stop when the sensor detects an object (digital input from the motor PDO communication), the third part is returned to the same position as started. so we decided to implement the first part with Linear movement mode and the second part with Rapid movement mode. But we encountered many communications errors when Controller switches from Linear to Rapid mode. The motor needs to get SYNC0 signal and if it doesn't get for 3ms it makes motor stops with failure. so when switching from Linear to Rapid mode it seems that the SYNC0 signal is delaying. Now we switched the second part of the movement to linear mode but it requires that we move in small intervals and check between intervals which makes this movement much slower than what we need. is only Rapid mode provide an option to simultaneity move and interact with sensor digital input? Why we are suffering from communication problems when switching movements modes?
-
EtherCAT: ecatsdo write fails from terminal, works from etherlab
orhirshfeld replied to andyf's topic in Power PMAC
I switched the master to diagnosis mode and was able to view the SDO But I still have the issue to get this data when it's not in diagnosis mode -
EtherCAT: ecatsdo write fails from terminal, works from etherlab
orhirshfeld replied to andyf's topic in Power PMAC
I suddenly succeed in getting some SDO information until I mistype an address and it stops working, I attached a picture to illustrate it returned the following msg: " Error: BgThread sem_timedwait(emIoctlFinish_sem) timed out " I notice a suspicious configuration in my EtherCAT Configuration in Slave configuration -> Advanced Option -> SDO Access is set to 0, what does it mean that, is timeout disabled? or access to SDO is disabled? -
It worked like a charm I changed the ProgramData\DeltaTau permissions and now I can see the list I meant just the EtherCAT settings for viewing in IDE, I disconnect the network and import the ENI file to my project and now I can see all configurations but I'm not sure what would happen once I reconnect the PPMAC controller, is it going to load all EtherCAT configuration from ENI file to the controller? or it wouldn't change anything until I press "Load Mapping To PowerPmac" or "Build And Download All Programs" Also Another question: in Slave configuration -> Advanced Option -> SDO Access is set to 0, what does it mean that there is no timeout or access SDO is disabled? I'm asking it because I have problems to access SDO using ecattypedsdo() function you can see more info about ecattypedsdo() issue I'm encountering in my other post: http://forums.deltatau.com/showthread.php?tid=1063 Setting up EtherCAT involves making an ENI file for PMAC. If you use the built in copy of EC Engineer, the "Import Slaves" option will internally pass that ENI file. If you already have an ENI file, then you can use the "Import Slaves from ENI" option to browse for it. I'm not sure I understand, are you asking about just the ethercat settings?
-
I tried changing the permissions and got the same results by the way, in my PC it was installed by default in "C:/delta tau" path
-
We had some issue before reloading configurations Is it possible to load configuration only to the IDE project, for viewing and editing, without downloading to the PPMAC? What is the purpose of "Import Slaves from ENI"? is it just loading to IDE project? The loaded ENI files aren't Omron products, it's Axor Motor Mack Tron and Festo Fieldbus Module CTEU. FESTO-CTEU-EC ESI file: https://www.festo.com/net/el_gr/SupportPortal/default.aspx?documentId=273305&cat=4821 When importing any new ENI to the ESI Manager it's rebuilding cache and already imported file can be viewed in the ESI Manager but as soon as you close the ESI manager window and re-open and it would disappear. Festo CTEU-EtherCAT Modular - 20180719.xml.txt File_ETH_MKT_MKUN_Omron_rev2.xml.txt
-
I tried importing ENI but it seems unavailable I attached picture also from where I should import the ENI? is it "eni.xml" in the folder i uploaded from PPMAC? for example \192.168.0.136_16_6_15\Configuration\eni.xml also, as i asked above, why I don't see which ESI files I uploaded to the IDE using ESI Manager? thank you, Or Hirshfeld Control SW Engineer FFRobotics
-
EtherCAT: ecatsdo write fails from terminal, works from etherlab
orhirshfeld replied to andyf's topic in Power PMAC
Firmware version in IDE terminal: "vers 2.5.0.0" OS version in SSH terminal: "Welcome to Ubuntu 16.04.3 LTS (GNU/Linux 4.1.18-xenomai-2.6.5 i686)"