Jump to content
OMRON Forums

liaobp1983

Members
  • Posts

    1
  • Joined

  • Last visited

Everything posted by liaobp1983

  1. When previous technician said that Delta Tau (Umac Turbo) were going crazy in the past. I did not believe them. But now it happened to me twice in a row for different machine. (The other instance, I will post on another thread). Machine is running since for so long now (5 years). We have 3 cfg backup made through out these years. Yesterday, we decided to edit 6 lines of codes. For example M4017=1 to M4017=0. When I did a restore of the edited cfg, the machine did not run. I found that this is because IF(M4420=1) - M4420 must be equal to 1 for the machine to run. So using text editor, I find all for M4420 and the result is below: Line 2941: IF(M4420=1) Line 3628: AND(M4420=1) Line 3810: AND(M4420=1) Line 4107: OR(M4420=0) Line 4193: OR(M4420=0) Line 7966: AND(M4420=1) Line 8149: AND(M4420=1) Line 8432: OR(M4420=0) Line 8518: OR(M4420=0) Line 29630: M4420->* To my surprise. There is no code that will make M4420=1. So I add this code under PLC 1. My question are: 1) How the hell did the machine run for 5 years. Without this one line of code which is essential? 2) I did a backup, edit one line, make a restore of edited cfg. Now the machine is broke? make a restore of the backup cfg just made. Machine still broken?
×
×
  • Create New...