RafaelFalcaro Posted August 26 Share Posted August 26 Hi, I have a stepper configured on PowerPMAC BrickLV Firmware 2.5.4.0, using a biss-c 32-bit encoder as position feedback, configured as follow: Encoder: Acc84B[0].Chan[2].SerialEncCmd = $2114A0 EncTable[13].type = 2 EncTable[13].pEnc = Acc84B[0].Chan[2].SerialEncDataA.a EncTable[13].pEnc1 = Acc84B[0].Chan[2].SerialEncDataB.a EncTable[13].index1 = 0 EncTable[13].index2 = 0 EncTable[13].index3 = 0 EncTable[13].index4 = 0 EncTable[13].index5 = 0 EncTable[13].index6 = 0 EncTable[13].ScaleFactor = -1 Motor (snippet): Motor[3].pEnc = EncTable[13].a Motor[3].pEnc2 = EncTable[3].a Motor[3].PowerOnMode = 4 Motor[3].AbsPosFormat = $00082008 Motor[3].pAbsPos = Acc84B[0].Chan[2].SerialEncDataA.a Motor[3].pAbsPos2 = Acc84B[0].Chan[2].SerialEncDataB.a Motor[3].AbsPosSF = -1 I'm facing a problem with power on position settings, due to overflow on Acc84B[0].Chan[2].SerialEncDataA register. There are two experiments of executing #3hmz command on terminal on two different positions of my stage course (see WatchWindow with SerialEncData registers): From position 1 to position 2, I executed a #3j+ command on terminal, and after some seconds, I executed #3j/ and #3hmz commands. The expected behaviour on position 2 is a positive value, not the overflow seen in the test. Is there a power on position setting which fix this problem? Quote Link to comment Share on other sites More sharing options...
RafaelFalcaro Posted August 27 Author Share Posted August 27 Hi, I fixed the problem by changing: Motor[3].AbsPosFormat = $01082008 Quote Link to comment Share on other sites More sharing options...
MoMo Posted August 27 Share Posted August 27 I think your encoder conversion table does not need to use type=2. Generally speaking, when it is used as an incremental position, you only need to obtain the low-bit data. The absolute value position only needs to be obtained when the system is started. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted August 28 Share Posted August 28 What MoMo says is very true. A type 2 ECT entry to read the second register is not necessary unless it is possible for the source data to change by half the range or more of the “SerialEncDataA” 24-bit register in a single servo cycle. In this case a type = 1 single register read is recommended, as it saves both hardware access time, and software computation time. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.