Jump to content
OMRON Forums

Libraries and CPLC's


gerardo64
 Share

Recommended Posts

Hello,

from other older threads I saw that the only way to use functions located in other C-files, together with the CPLC's, would be to to use them as "Libraries".

It was told also that in Version 1.5 it was not yet supported, but it would be in the future.

 

Meanwhile, I have IDE V1.6.0.43 installed on my laptop & tried to call from the rticplc a small test function, declared in rticplc.c as "extern" and with the body located in a file below "Libraries". It worked fine, no errors.

 

My question: was it a fortune case that it worked or does it generally work now with 1.6.0.43? Or is there another possibility of having many source files working with rticplc.c (without having to include them, as in older versions of IDE)?

Thanks & regards

Gerardo

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Guest
This topic is now closed to further replies.
 Share


×
×
  • Create New...