Jump to content
OMRON Forums

Acc5E3 I/O


KennNova

Recommended Posts

  • Replies 3
  • Created
  • Last Reply

Top Posters In This Topic

Under the heading IO Port Setup, the manual describes how to configure the general purpose IO as either inputs or outputs and inverting or non-inverting. For an inverting I/O point, 0=+5V and 1=0V, and for a non-inverting I/O point, 0=0V; 1=+5V. It is TTL logic. A connection diagram would be helpful, wouldn't it? We are getting those into the I/O manuals now as they are created or revised.
Link to comment
Share on other sites

Under the heading IO Port Setup, the manual describes how to configure the general purpose IO as either inputs or outputs and inverting or non-inverting. For an inverting I/O point, 0=+5V and 1=0V, and for a non-inverting I/O point, 0=0V; 1=+5V. It is TTL logic. A connection diagram would be helpful, wouldn't it? We are getting those into the I/O manuals now as they are created or revised.

 

Thanks Greg. The TTL signal level is a show stopper for us. 5 volt logic is pretty much useless in our market of industrial control. We'll have to go another route for the extra I/O we need.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...