Soder Posted March 6, 2014 Share Posted March 6, 2014 Hi, I have been developing a position capture application with 2 stepper motors with built in encoders. Now I have moved to 2 stepper motors but without encoders. This is going to be used for demonstration purpose of the application only, in the end there will probably be encoders anyway. When I had the encoders everything worked fine, but since there are no encoders in the new setup there aren't any position to capture. Therefore I would like to set up a pseudo-closed loop for the new setup to be able to demonstrate the application. I know I have to set: I7mn0=8, and probably set I7mn6=2 to output the PFM, but I am not sure. I tested it by reading M101 for the current position. But as soon as the motor is moved the position endlessly increments/decrements. I also tried changing some PID parameters according to this suggestion: http://forums.deltatau.com/showthread.php?tid=310&highlight=Pulse+and+Direction But I had the same result. How do I properly setup the pseudo-loop? Thanks a lot. If my information is insufficient please tell me what to I need to add. Link to comment Share on other sites More sharing options...
Soder Posted March 7, 2014 Author Share Posted March 7, 2014 Just noticed I have to change: I102 from $078002 to $078004 But this breaks everything. I can't move the motor. Other important variables might be: I103=$350B I104=$350B I105=$35C0 From what I can see from the Software reference manual I103 and I104 are non standard. I got this configration from a colleague. Trying to find out what they changed. Also worth mentioning is that this is a Geo Brick LV IMS-II. Link to comment Share on other sites More sharing options...
steve.milici Posted March 7, 2014 Share Posted March 7, 2014 Please contact one of our Technical Support engineers at support@deltatau.com with your current setup details. Link to comment Share on other sites More sharing options...
Soder Posted March 10, 2014 Author Share Posted March 10, 2014 Done, feel free to remove this thread. Link to comment Share on other sites More sharing options...
Recommended Posts