GuitarBrad Posted February 14, 2018 Share Posted February 14, 2018 Using Setup Pro2 to setup UMAC/TurboPMAC2 w ACC24E2A. The ACC24E2A's channels 1 & 2 are dead, but 3 & 4 work. I have a 2 axis application, so what the heck. I bring up Setup Pro 2, and start configuring, leaving Motor 3 as channel 3 and Motor 4 as channel 4. The actual motors and amps are identicle. Motor 3 has pos and neg limit switches. I get through configuring it just fine, Open loop test, a nice graph. Motor 4 has no limits switches, so I disable position limits, otherwise the setup is the same as 3, and try and run Open Loop test, it complains about the positive position limit being true so it wont run?? The channel 4 front panel connector is empty! I even stuck channel 3's limits connector into channel 4, still complains? entering open loop mode on motor 4 in terminal works? I'm about to try again except make channel 3 motor 1, 4 motor 2 or am I wasting my time, (the ACC24 has problems), is there no other explaination other than a whacked board? UPDATE: not the board, quirky bug in Setup Pro2 Link to comment Share on other sites More sharing options...
steve.milici Posted February 16, 2018 Share Posted February 16, 2018 This could be due to bad hardware. It could also be “non-standard” setup issues with the software. Contact the ODT Technical Support Group for further assistance: support@deltatau.com Link to comment Share on other sites More sharing options...
Recommended Posts