Jump to content
OMRON Forums

Coordinate systems D-variables


marcelo.moraes

Recommended Posts

Hi,

 

Is it possible to configure a global variable from communication-thread D-variables?

 

I cannot access the position readback of virtual axes individually from a PLC file, and I don't know why. I just want to map a readback position to a Q variable, but it is not that easy from a PLC file...

 

The only thing I want is the numerical response for one axis, not string for all axes like the output for "&1p" command.

 

Example:

 

&1p

X111 Y222 // string output with all axes set in D0 mask

&2p

X333 Y444

 

I can access the desired values with commands like:

 

&1D // Apply "CS1 environment" to D-variables

X111 Y222

D6 // Query CS1 axis X position

111 // this is the output I want

D7 // Query CS1 axis Y position

222 // this is the output I want

&2D;D7 // Change D-variables to CS2 environment; query for CS2 Y position

X333 Y444 // first command output (undesired)

444 //second command output (desired)

 

But these commands only work from communications threads / scripts other than PLC files.

So I tried to access from PLC file the D-variables from coordinate systems and PLCs, but these are different domains.

 

What I am missing? How can I access these values from PLC?

 

Controller: Power Brick LV

 

 

Best regards,

Marcelo Moraes

Link to comment
Share on other sites

  • Replies 2
  • Created
  • Last Reply

Top Posters In This Topic

If you issue the equivalent buffered program command (pread) from inside a program, you can access the results directly with D6, D7, etc. from within the same program (top-level program or its subroutines).

 

If you want to access these values from outside that particular program, you can use the full data structure name. If the command was issued from a PLC program, you can use Plc[n].Ldata.D[6] etc. If the command was issued from a motion program, you can use Coord[x].Ldata.D[6] etc.

 

You cannot access the local variables of a communications thread from outside that thread.

Link to comment
Share on other sites

  • 3 weeks later...
Guest
This topic is now closed to further replies.

×
×
  • Create New...