Goal: Change parameter settings in the ARCL command line.
Problem: When I try to make any kind of parameter changes I get the same error. Below is an example of when I attempt to change the robot width.
Config had at least this problem: line 11426: width not in section, client needs an upgrade.
Background: I have used the "getConfigSectionList" & "getConfigSectionInfo" to identify the parameters that can be changed. So the command should work. I have also updated the mobileplanner software to allow parameter changes to be made using ARCL.
Current Code:
Configstart
Configadd general
Configadd width 400
ConfigParse
Omron LD60/90
in Pre-Turbo PMAC
Posted
Goal: Change parameter settings in the ARCL command line.
Problem: When I try to make any kind of parameter changes I get the same error. Below is an example of when I attempt to change the robot width.
Config had at least this problem: line 11426: width not in section, client needs an upgrade.
Background: I have used the "getConfigSectionList" & "getConfigSectionInfo" to identify the parameters that can be changed. So the command should work. I have also updated the mobileplanner software to allow parameter changes to be made using ARCL.
Current Code:
Configstart Configadd general Configadd width 400 ConfigParse