andreslobo
-
Posts
6 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by andreslobo
-
-
Just bought another backup board for my ancient press brakes.
1. This board is sn 8417 and it has a much larger eeprom for the firmware on the daughter board. Can I flash this with my pe win just like the other ones I have?
2. The board arrived without the metal tab that wraps around the 60 pin connector and locates it in the PC backplane. Can I buy one? If so where?
-
[quote='Sina' pid='651' dateline='1282664488'] Here is the manual for PMAC-PC boards (602191). Sina Thanks so much and I will contact them for firmware. I am pretty certain that I now have enough information to do a board swap when that dark day arrives.
-
Sina Looked at the back of the board, it is a 602191-103 serial number 9632 with a 602705-103 daughter board sn 331. I'd appreciate info on it as well as a copy of firmware # 1.16D with a date of 11-10-97
-
[quote='Sina' pid='645' dateline='1282582361'] The part numbers are usually a 6 digit number starting with 602xxx or 603xxx. [/quote] Sina Thanks much for the info. I set the jumpers the same on both boards, pulled one from the rack and replaced it with the new one. It was recognized by pewin, had the green and yellow led lights on. But where the heck do I find the part number on the board. On the base board I can only find pmac pc, are the numbers hidden under the daughter board?[hr] Sina Looked at the back of the board, it is a 602191-103 serial number 9632 with a 602705-103 daughter board sn 331. I'd appreciate info on it.
-
I have several old electric presses, all with Pmac pc 4 channel boards in them. As a part of risk management I bought a used Pmac pc with a pmac pv cpu to have as a swap out replacement just in case. From the limited reading I have done it appears as though it is 8 channel. The question is, if I set the jumpers the same as the old board, load the same firmware as the old board (everything is flash and I have the motion program), download the pmac programs, and plug it in should it work? Thanks in advance
Info and parts needed for PMAC PC board
in Pre-Turbo PMAC
Posted
the main board part number is 602191-103
The daughter board is 602398-100 sn 3941