Telnet fails in Turbo PMAC Posted November 29, 2011 Hi, I can connect to the PMAC via Pewin32PRO2 successfully, but cannot telnet to it. Pinging the IP address works. I've changed the IP address from the factory default. I have never been able to telnet successfully before. I'm running Win XP. Do I need to configure the PMAC somehow to allow telnet? I get the following error when trying to telnet : C:\Documents and Settings\nia>telnet 134.79.218.31 Connecting To 134.79.218.31...Could not open connection to the host, on port 23: Connect failed Thanks! Nia
Telnet fails
in Turbo PMAC
Posted
Hi,
I can connect to the PMAC via Pewin32PRO2 successfully, but cannot telnet to it. Pinging the IP address works.
I've changed the IP address from the factory default. I have never been able to telnet successfully before. I'm running Win XP.
Do I need to configure the PMAC somehow to allow telnet?
I get the following error when trying to telnet :
C:\Documents and Settings\nia>telnet 134.79.218.31
Connecting To 134.79.218.31...Could not open connection to the host, on port 23:
Connect failed
Thanks!
Nia