Jump to content
OMRON Forums

G. BAUTISTA

Members
  • Posts

    2
  • Joined

  • Last visited

Recent Profile Visitors

The recent visitors block is disabled and is not being shown to other users.

G. BAUTISTA's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Thanks Vince: When you said "Be sure your coordinate system definitions is defined for CTS/MM (Pulses Per Unit in the AutoPilot first page). " I don´t know if you refer to the comment bellow the screen. It appears : "X axis definition. Encoder counts per unit (inch/MM) for X axis" for example? About the PPU calculation if I am working in mm, the Unit Conversión factor (25.4 mm/inch) is used or not? regards
  2. HI: I HAVE A ADV 900 WITH BRICK CONTROLLER. IN THE CNC AUTOPILOT PROGRAM, IN THE AXIS MOTOR WINDOW I SELECTED METRIC(mm) AND IN THE STD. PLC WINDOW I SELECTED IN HANDLE SECTION: ENABLE AND MAX INCREMENT 1.000 AND MIN INCREMENT 0.01. WHEN I OPEN THE HMI IN THE PMAC-NC PRO2 RUN TIME, IN THE OPERATION MODE SECTION IF I SELECT THE HAND/INC KEY APEAR: MANUAL X HANDWELL 0.000100 INCREMENTAL 0.000100 WITH THE LO POSITION IN THE SELECTOR. IF I CHANGE IT AT MED POSITION APEAR NOW: MANUAL X HANDWHEEL 0.010000 INCREMENTAL 0.01000. IT SHOWS THE VALUES AS IF I AM WORKING IN INCH. HOW I CAN CHANGE THIS ? THANK FOR YOUR HELP. I WISH EXPLAIN THE PROBLEM CORRECTLY GILBERTO BAUTISTA MEXICO, CITY
×
×
  • Create New...