G. BAUTISTA
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by G. BAUTISTA
-
-
HI:
I HAVE A ADV 900 WITH BRICK CONTROLLER.
IN THE CNC AUTOPILOT PROGRAM, IN THE AXIS MOTOR WINDOW I SELECTED METRIC(mm) AND IN THE STD. PLC WINDOW I SELECTED IN HANDLE SECTION: ENABLE AND MAX INCREMENT 1.000 AND MIN INCREMENT 0.01.
WHEN I OPEN THE HMI IN THE PMAC-NC PRO2 RUN TIME, IN THE OPERATION MODE SECTION IF I SELECT THE HAND/INC KEY APEAR:
MANUAL X HANDWELL 0.000100 INCREMENTAL 0.000100 WITH THE LO POSITION IN THE SELECTOR. IF I CHANGE IT AT MED POSITION APEAR NOW: MANUAL X HANDWHEEL 0.010000 INCREMENTAL 0.01000.
IT SHOWS THE VALUES AS IF I AM WORKING IN INCH. HOW I CAN CHANGE THIS ?
THANK FOR YOUR HELP. I WISH EXPLAIN THE PROBLEM CORRECTLY
GILBERTO BAUTISTA
MEXICO, CITY
HANDWHELL INCREMENT
in PMAC NC PRO2
Posted
Thanks Vince:
When you said "Be sure your coordinate system definitions is defined for CTS/MM (Pulses Per Unit in the AutoPilot first page). " I don´t know if you refer to the comment bellow the screen. It appears : "X axis definition. Encoder counts per unit (inch/MM) for X axis" for example?
About the PPU calculation if I am working in mm, the Unit Conversión factor (25.4 mm/inch) is used or not?
regards