Jump to content
OMRON Forums

G. BAUTISTA

Members
  • Posts

    2
  • Joined

  • Last visited

Posts posted by G. BAUTISTA

  1. Thanks Vince:

     

    When you said "Be sure your coordinate system definitions is defined for CTS/MM (Pulses Per Unit in the AutoPilot first page). " I don´t know if you refer to the comment bellow the screen. It appears : "X axis definition. Encoder counts per unit (inch/MM) for X axis" for example?

     

    About the PPU calculation if I am working in mm, the Unit Conversión factor (25.4 mm/inch) is used or not?

     

    regards

     

     

    Be sure your coordinate system definitions is defined for CTS/MM (Pulses Per Unit in the AutoPilot first page).

     

    Then you can modify the Handwheel increments in the CNTPANEL.PLC via the following code to make the increment whatever you want (The following is for 0.0001 - 1.0000):

     

    //------- Distance selection Logic

    //If the user wants to change the HANDLE INCREMENT...

    //THIS IS THE SECTION where the INCREMENT values can be set.

    //----------------------------------------------------------------------------

    IF (C_DIST_M > 0)

    IF (C_DIST_M = SEL_DIST_10000)

    VS_HAND_STEP_M = 1.0000

    VS_JOG_STEP_M = 1.0000

    S_DIST_M = C_DIST_M

    ELSE IF (C_DIST_M = SEL_DIST_1000)

    VS_HAND_STEP_M = 0.1000

    VS_JOG_STEP_M = 0.1000

    S_DIST_M = C_DIST_M

    ELSE IF (C_DIST_M = SEL_DIST_100)

    VS_HAND_STEP_M = 0.0100

    VS_JOG_STEP_M = 0.0100

    S_DIST_M = C_DIST_M

    ELSE IF (C_DIST_M = SEL_DIST_10)

    VS_HAND_STEP_M = 0.0010

    VS_JOG_STEP_M = 0.0010

    S_DIST_M = C_DIST_M

    ELSE IF (C_DIST_M = SEL_DIST_1)

    VS_HAND_STEP_M = 0.0001

    VS_JOG_STEP_M = 0.0001

    S_DIST_M = C_DIST_M

    ENDIF ENDIF ENDIF ENDIF ENDIF

    C_DIST_M = 0

    ENDIF

    60930427_systemdefinition.thumb.jpg.e7e2c072fc90b0c051e4c44519d8aaa7.jpg

  2. HI:

    I HAVE A ADV 900 WITH BRICK CONTROLLER.

    IN THE CNC AUTOPILOT PROGRAM, IN THE AXIS MOTOR WINDOW I SELECTED METRIC(mm) AND IN THE STD. PLC WINDOW I SELECTED IN HANDLE SECTION: ENABLE AND MAX INCREMENT 1.000 AND MIN INCREMENT 0.01.

     

    WHEN I OPEN THE HMI IN THE PMAC-NC PRO2 RUN TIME, IN THE OPERATION MODE SECTION IF I SELECT THE HAND/INC KEY APEAR:

    MANUAL X HANDWELL 0.000100 INCREMENTAL 0.000100 WITH THE LO POSITION IN THE SELECTOR. IF I CHANGE IT AT MED POSITION APEAR NOW: MANUAL X HANDWHEEL 0.010000 INCREMENTAL 0.01000.

     

    IT SHOWS THE VALUES AS IF I AM WORKING IN INCH. HOW I CAN CHANGE THIS ?

     

    THANK FOR YOUR HELP. I WISH EXPLAIN THE PROBLEM CORRECTLY

     

    GILBERTO BAUTISTA

    MEXICO, CITY

×
×
  • Create New...