biocat
-
Posts
7 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by biocat
-
-
The Power PMAC was upgraded and assembled by Delta Tau fully. I haven't investigated it. Will give a shot!
Thank you!
-
I use 115200 baud rate, 8 data bits, 1 stop bit, None for parity, and XON/XOFF for flow control. That output you are getting looks very strange, I'm not sure what is going on there. I attached an image of what my console looks like on powerup.
Wonderful! Thank you! 115200 works. I used 9600 wrongly. I guess my kernel has problem. It keeps rebooting in every 180 seconds.
-
Could you tell me what is your configuration of the serial line to COM? Such as the serial line Speed(baud), Data bits, Stop bits, Parity and Flow control.
Thank you!
-
Thank you for your reply. Have you tried to use RS 232 to USB converter to connect to Power PMAC? Did it work too?
-
I have a Power PMAC which has worked normally. After I powered cycle Power PMAC and re-plugged the Ethernet cable, I found its IP address lost. To get the real IP address from Power PMAC, I used a USB memory stick and rebooted Power PMAC. The folder 'PowerPmacIP' was empty. No data saved in USB memory stick. Same as SD memory card. I have no RS 232 handy to try it. But I'm afraid it lost IP address already. What should I do? Can I assign an IP address to it? How to do it?
In users' manual, it said an IP address entered by user in IDE does not set or change the IP address of the Power PMAC; it simply specifies the IP address at which the IDE will attempt to communicate. After I set IP address in IDE and click 'Apply permanently' button, the Power PMAC IP address was changed or not. Why I can't find its IP address? Even I tried the default IP address, 192.168.0.200 to connect by Ethernet, it didn't work either.
-
I'm using Power PMAC IDE to do Test and Commission the motor. My hardware are ACC-24E2A and AMP-1 4-axis linear amplifier. This servo motor has been tested in other channels without problem. But in one channel, I got the Debug Message as below. Even I changed the direction, it still didn't work. Could somebody help me? Thanks!
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Arguments Entered:
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Motor Number: 2
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Maximum open loop command percentage: 100.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop command duration (msec): 800.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Number of iterations: 2
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 20.000000% command output
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 40.000000% command output
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 60.000000% command output
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 80.000000% command output
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 100.000000% command output
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 120.000000% command output
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Feedback direction didn't match the commanded output direction!
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Continuing with the setup with current settings can be dangerous.
11/19/2012 :3:48 PM - xxx.xx.xxx.xxx, Module - Set Motor : Please change the direction of feedback and start the test over again.
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - FeedbackSetup : Graph Control Connected
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Graph Control Connected
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Arguments Entered:
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Motor Number: 2
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Maximum open loop command percentage: 100.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop command duration (msec): 800.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Number of iterations: 2
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 20.000000% command output
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 40.000000% command output
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 60.000000% command output
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 80.000000% command output
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 100.000000% command output
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Open loop test with 120.000000% command output
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Measured velocities :
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Positive velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Negative velocity: 0.000000
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Feedback direction didn't match the commanded output direction!
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Continuing with the setup with current settings can be dangerous.
11/19/2012 :3:49 PM - xxx.xx.xxx.xxx, Module - Set Motor : Please change the direction of feedback and start the test over again.
IP address lost and recovery?
in Power PMAC
Posted
Thank you, Shansen, for letting me know. Too bad we have the same problem. I was told it's the memory partition issue.
I will try your solution later on.
Many thanks!