Power PMAC
Discussions about Power PMAC products (including UMAC Accessories, Power Brick products, Power Clipper, CK3x products, and more) along with their software, including Power PMAC IDE, NC16 HMI, and Power PMAC PDK.
Subforums
2,193 topics in this forum
-
- 6 replies
- 4.3k views
As of late 2020, the locations for the firmware and IDE have moved. Previous versions of both are still being kept on the Delta Tau website, available through the for firmware (forums account required) and the Software Center Updates page for software. However, the distribution methods for each have changed for future versions.http://forums.deltatau.com/filedepot/ [FILE REMOVED] Future versions of the IDE are available instead from the Omron Industrial Automation website: https://automation.omron.com/en/us/products/family/PMAC%20IDE Future versions of firmware can typically be distributed directly to customers through Omron Distributors rather than being available …
Last reply by Alex Anikstein, -
- 1 follower
- 0 replies
- 1.2k views
In some cases customers may not be able to connect to Power PMAC ARM through the USB-Serial UART Diagnostic Port over a Micro-USB cable. In this case, after pressing the button to put the port into serial mode, the CPU appears in the device manager as "FX230X Basic UART" instead of receiving a COM port. To fix this issue, install the appropriate version of this driver. (Windows 32 or 64 bit) https://www.ftdichip.com/Drivers/D2XX.htm
Last reply by Eric Hotchkiss, -
- 2 replies
- 16.3k views
I thought that posting the excerpt (attached) from the Power PMAC Training Slides, "Talking to Power PMAC," might be helpful here as a quick reference covering most questions regarding communicating with Power PMAC. For the rest of the training slides please visit and click Power PMAC-->Training Slides.http://forums.deltatau.com/filedepot/ [FILE REMOVED] Talking to Power PMAC 2012-02.pdf
Last reply by Omron Forums Support, -
- 0 replies
- 8.4k views
Attached to this post is a list of Power PMAC parameters equivalent (or almost equivalent) to Turbo PMAC's I-Variables.Power PMAC Turbo I-Variable Equivalents 2014-01.pdf
Last reply by Omron Forums Support, -
- 1 follower
- 3 replies
- 66.7k views
The Power PMAC training slides contain useful examples covering many of the Power PMAC's new features. The following link takes you to FileDepot, so after clicking the link, click "Power PMAC" and then "Training Slides." http://forums.deltatau.com/filedepot [FILE REMOVED]
Last reply by Sina.Sattari, -
- 2 followers
- 1 reply
- 70k views
This post contains the Power PMAC software reference and user manual. Note these files are updated frequently. http://forums.deltatau.com/filedepot [FILE REMOVED]
Last reply by Sina.Sattari, -
hello. I have a question about how to use Dynamic Break in TurboPMAC, ACC-24E2 + ServoTronix CDHD PWM Drive combination. In this project, we plan to use a combination of PowerPMAC (ArmCPU) and ACC-24E3 ServoTronix CDHD PWM Drive. It seems that there are parts that change as the CPU changes. When I searched the SRM document, it was identified as the AdcStrobe variable when using Gate1 and the AdcAmpCtrl variable in the case of Gate3. Please inquire about how to use this function. Documents previously referenced are attached separately. ServiceChannelCommand.txt, ServiceChannelQuery.txt The code I used based on the attached document is as follow…
Last reply by steve.milici, -
- 3 followers
- 8 replies
- 7.2k views
Is there a better way to save normal user variables other than either adding them to the pp_custom_save.tpl or going into the ppmac, uploading the pp_save.tpl, modifying it, and downloading it? Sina posted directions to upload the pp_save.tpl from the IDE a couple of years ago, but it no longer seems to work.
Last reply by steve.milici, -
- 2 followers
- 1 reply
- 18 views
We support machines that have varying hardware, but otherwise operate mostly the same. In particular I'm thinking about servo motors/amplifiers (and even gear-drives with differing gear ratios). We've been supporting some of these machines for over 20 years, and others are only a couple years old or even newer. As products are phased out, we are forced to change to newer parts with different characteristics, and the software must adapt to this. We are now at the point where Turbo PMAC Clipper is not really available anymore, so we are working on moving over to CK3M. As some of the older machines have components fail, we must upgrade them with parts that are currently…
Last reply by David White, -
- 1 follower
- 1 reply
- 17 views
Hi, I would like to ask how to change the resolver direction in PowerBrick LV. I followed the User's Manual: Motor[].PhaseOffset = – present value Motor[].PwmSf = – present value PowerBrick[].Chan[].EncCtrl = the opposite decode of the present value (e.g. 7 or 3) If using resolver or halls absolute power-on phasing: Motor[].AbsPhasePosSf = – present value Motor[].AbsPhasePosOffset = 2048 – present value If using resolver absolute power-on position: Motor[].AbsPosSf = – present value After that, I downloaded the code, read absolute position, did manual phasing. Phasing successfully However, the resolver direction did not change. Do you have any id…
Last reply by steve.milici, -
- 1 reply
- 40 views
Dear Sir, We have CK3M ETHERCAT CPU-111 + AX1515n + MD7110 + MD7120 installed for a 6 axis Reshrpening Machine. 5 servo's are of Delta ASDA-A2-E 1Khz Ethercat and 1 VFD for Spindle. we are facing certain problems in configuring and using the setup which are as follows. the PC config is Advantek Indl. core I7 CPU with 8gb ram and 1th SSD. with win 64bit OS. 1) Power Pmac IDE 4.3 hangs frequently after configuring and Tuning delta asda-a2-e EtherCat Motors on Windows 8.1 pro and win 7 64bit. Kindly suggest proper system cpu frequency settings. currently we used 4khz phase and 1khz servo freq, 2) initially first AX15…
Last reply by Alex Anikstein, -
- 1 follower
- 1 reply
- 47 views
Hello. I'm using PMac APM CPU (485). I need to sizing up my memory, because i need to download 500MB size NC-Code. After i size up memory to 510MB, Download, Save, ReBoot, WatchDog has red light, and My Power PMac doesn't working. Can't connect by PMac IDE. i tried to initialize PPMac, by taking off my Axis Control Card, Reboot. but it does not working. Is there anyway to initialize my Power PMac? I can't use pmac ide S/W Because, in PMac IDE, i can't connect to my PPMac. i ping to 192.168.0.200 by CMD. it was responded. if anyone has anything solution about this, le…
Last reply by steve.milici, -
- 2 followers
- 5 replies
- 207 views
Dear All, I'm trying to save a project after building and downloading successfully. Unfortunately, it throws a list of error stating that the files are READ-ONLY. Also the variables created are accessible until PMAC is powered off. Once powered OFF all the parameters are missing. Can I know what causes these issues? Thank you.
Last reply by steve.milici, -
- 2 replies
- 41 views
I have a lathe project where the operator wants the zero position to be in the middle of the chuck and the home position to be at the beginning of the travel where the home switch is. I currently have it programmed to perform a home search move until it hits the home switch but then the zero is not in the center where they want it. Is there an effective way to do this without installing a switch in the middle of the travel? thank you
Last reply by Curt Wilson, -
- 2 replies
- 35 views
Here is a sample of the code I am trying to run. The tool will move to the correct offset position, will spiral down to -0.180, completing the second line of the spiral, then it simply stops and I have an error. Error Status: Illegal move mode or command while cutter compensation active. G55 G17 G20 G40 G49 G80 G90 M6 T5 (.5 FINISH) M1 G43 H5 G53 Z0.0 M3 S2000 M8 G0 G90 X-4.0 Y0.0 Z3.0 G42 D5 G1 X-4.1885 Y0.0635 F5.0 Z1.0 F30.0 M1 G1 Z0.1 G3 X-4.1885 Y0.0635 Z-0.090 I0.0 J-0.0635 F4.0 G3 X-4.1885 Y0.0635 Z-0.18 I0.0 J-0.0635 F4.0 G3 X-4.1885 Y0.0635 Z-0.27 I0.0 J-0.0635 F4.0 G3 X-4.1885 Y0.0635 Z-0.35 I0.0 J-0.0635 F4.0 …
Last reply by DC Padgett, -
- 1 reply
- 36 views
Im wondering the best way to be able to add a tool offset on linear axis I can seem to find the correct command. For instance a tool with a .1 offset should be able to input .1 in the axis offset and the position will stop .1short. Thanks
Last reply by chrisvk, -
- 1 reply
- 86 views
I'm seeing references on the Omron website on the Power PMAC IDE page to a new IDE version 4.6.0.14 released back in May .. there are software release notes as well as some "Product News" / "Power PMAC IDE Modification Notice" .. but don't see the actual IDE version there to be downloaded. Is there some alternate place to download the new version from?
Last reply by Alex Anikstein, -
- 1 follower
- 2 replies
- 90 views
Hi Ck3m cpu101 firmware version 2.6.1.0 How can I communicate using NX-EIC202 ethernet ip protocol.
Last reply by fatihbeyy, -
The homing reference index of Motor[4] is changed to the TTL signal accessed by Acc24E3[1].Chan[0]; pCaptFlag and pCaptPos change from Acc24E3[0].Chan[3] to Acc24E3[1].Chan[0] as the reference signal, the configuration is as follows: Motor[4].pCaptFlag=Acc24E3[1].Chan[0].Status.a //Modified Motor[4].pCaptPos=Acc24E3[1].Chan[0].HomeCapt.a//Modified EncTable[4].pEnc = Gate3[0].Chan[3].ServoCapt.a EncTable[4].pEnc1 = Gate3[0].Chan[3].AtanSumOfSqr.a Motor[4].pEnc = EncTable[4].a; Motor[4.pEnc2 = EncTable[4].a; Motor[4].pEncCtrl =Acc24E3[0].Chan[3].OutCtrl.a Motor[4].pEncStatus=Acc24E3[0].Chan[3].Status.a The bad problem is…
Last reply by zerbzhang, -
- 2 followers
- 1 reply
- 172 views
It appears PPMAC originally did not support negative case constants in switch structures. However, the firmware update history for V2.5 Release Updates (August 2018) includes the following note: But when I try to use code such as the following, I get a Syntax Error on the minus sign: Has the IDE just not been updated to support this change yet? Is there a different syntax I should use here? Or am I misreading the history note and this is actually not supported?
Last reply by steve.milici, -
- 2 followers
- 8 replies
- 239 views
I am troubleshooting an issue related to a servo motor which we use to drive a monochromator Bragg axis. At a specific range of the motion, we observe that the x-ray beam jitters possibly due to motor oscillation. The motor is driven by an external amplifier and we use power PMAC for torque control. The motion is typically carried out by executing a motion program. We first observe the issue with our data. Afterwards we jogged the motor in the questionable range and was able to narrow down on the range where we see the oscillation. The x-ray beam stabilize upon killing power to the motor. I am guessing that the motor is trying to correct its position during this range. In…
Last reply by cdesilva, -
- 1 follower
- 1 reply
- 84 views
I remember there is a setting to reduce the velocity in all motors but I can't find it in the manuals. All the motors are moving slowly so I suspect someone set this in the terminal. Thanks.
Last reply by David White, -
- 2 followers
- 4 replies
- 137 views
Dear All, I'm working on a three axes system with two vector feedrate linear axes (X&Z) and one rotary C axis. I would like to know how to set the three axes to move synchronised based on a given feedrate? Currently if running C-axis alone, provides a max feedrate of 1 motor unit/ min. Can anyone suggest the best practice to assign and synchronize axes motion? Thank you.
Last reply by Eric Hotchkiss, -
- 2 followers
- 3 replies
- 103 views
I am running a real time PLC that is stuffing position data into registers that I can read from later. I'd like to filter the positions to take random out . My plan was to make a simple average. Is there a feature in PowerPMAC that can already do this for me, or do I need to roll my own? How fast is the RTI PLC operating (or how can I look it up on my machine?). I am reading the data around 2000 Hz, so I need to make sure my running average is a lot faster than that.
Last reply by Eric Hotchkiss, -
- 2 followers
- 2 replies
- 200 views
This is going to get a little long in the tooth, my apologies... I have converted Turbo PMAC (Clipper) software to Power PMAC for use with CK3M as I've been told Clippers are very hard to get anymore. Traditionally we used the Restore menu option in PEWIN32Pro to load a single .CFG file we update (there are actually several files for different machine variations we sell). We never did get into include-files, so everything is self contained in a single .CFG. As you can probably imagine, this makes quick edits/variable updates quite easy for non-experts to accomplish. As we are moving toward using Power PMAC in our machines, I'm wondering about best practices for manag…
Last reply by Ian Nicholson,