Omron Support Team Posted September 25, 2012 Share Posted September 25, 2012 I thought that posting the excerpt (attached) from the Power PMAC Training Slides, "Talking to Power PMAC," might be helpful here as a quick reference covering most questions regarding communicating with Power PMAC. For the rest of the training slides please visit and click Power PMAC-->Training Slides.http://forums.deltatau.com/filedepot/ [FILE REMOVED]Talking to Power PMAC 2012-02.pdf Quote Link to comment Share on other sites More sharing options...
johann Posted May 15, 2013 Share Posted May 15, 2013 I thought that posting the excerpt (attached) from the Power PMAC Training Slides, "Talking to Power PMAC," might be helpful here as a quick reference covering most questions regarding communicating with Power PMAC. For the rest of the training slides please visit and click Power PMAC-->Training Slides.http://forums.deltatau.com/filedepot/ [FILE REMOVED] Thanks. I wonder if it is possible to load programs (and execute them) through telnet or accessing the embedded web server in the Power PMAC... Quote Link to comment Share on other sites More sharing options...
Omron Support Team Posted April 15, 2015 Author Share Posted April 15, 2015 Hi, Yes, it's possible. You just open communication with Power PMAC through SSH, issue gpascii -2, and then you can download the programs directly there. Note that this technique will not work if named local variables are present within the motion program. You need to have predefined the local variable names using #defines, then download them to PMAC through the IDE, before you can use them. This is because all name-to-index conversion for variables is done at download time through the IDE only. I do not suggest using the embedded web server as it is designed for very basic functionality only, such as polling positions. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.