Jump to content
OMRON Forums

dhidas

Members
  • Posts

    4
  • Joined

  • Last visited

dhidas's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Thanks, this looks to be what I was after! (small correction is a missing : after u.user): ptr LENC1CRC->u.user:$3000.4.1
  2. I'm looking to use it in a PLC (script language)
  3. I'd like to have a shorthand way to look at the bits in SerialEncDataB, for example looking at the CRC bit etc. I thought something like this might work, but it doesn't seem to. Is there a good way to do this without having to do all of the bit shifting in a PLC? #define LENC1CRC Acc84E[0].Chan[0].SerialEncDataB.22.1
  4. Hello, I am using direct microstepping on #1 of a GeoBrick LV and wish to use the position compare functionality as a trigger of sorts (in this case step as there is no encoder). I setup #5 as a virtual motor following the instructions for PFM so that I could use the position compare on #5 when it is following #1. The problem I am currently having is that #5 lags significantly behind #1 at higher speeds. I tried setting program acceleration and velocity to high values, the s-curve and accl-times to very small values for #5, and upped the PFM frequency, but I see no change in the amount of following error. Is there any other way to make #5 more synchronized with #1? Thanks for your help, -Dean
×
×
  • Create New...