maslick
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by maslick
-
-
Hello!
I would like to control the hexapod platform using PVT mode. We have already implemented a system using LINEAR mode. Now, I have added into the inverse kinematics routine the computation of the motors' velocities.
Here is a piece of a motion program I have written so far:
close #include "macro_constants_def.pmc" open prog 1 ; open buffer for program entry clear ; erase existing contents of buffer &1 PVT200 ;Move absolute ABS ;Transform from uRad to deg. UCSPoseA=UCSPoseAuRad/TouRad UCSPoseB=UCSPoseBuRad/TouRad UCSPoseC=UCSPoseCuRad/TouRad X(UCSPoseX):(XVel)Y(UCSPoseY):(YVel)Z(UCSPoseZ):(ZVel)A(UCSPoseA):(AVel)B(UCSPoseB):(BVel)C(UCSPoseC):(CVel)
The only thing is that I use only one "X:(Vx)Y:(Vy):Z:..." statement. When I have to slice my entire move (contour) into pieces, so like the move will consist of 50 little jogs.
How can I implement this? By putting it in a loop? Or is there a better way?
Thanks in advance!
--
Best regards,
Pavel Maslov, MS
Controls Engineer at Pulsed power Lab
Efremov Institute for Electro-Physical Apparatus
St. Petersburg, Russia
Mobile: +7 (951) 672 22 19
Landline: +7 (812) 461 01 01
[hexapod] PVT
in Turbo PMAC
Posted
Hey Richard!
The axes velocities (X,Y,Z,A,B,C) have to be constant in my case and are set by the user.
Do you mean something like (using abstract syntax notation):