jamet
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by jamet
-
-
I am running a NC program. checking I5192 (CMR disable veriable) and M336 (CMR Bit) for every tool change. The bits stay I5192 = 0 and M336 = 1. Tool 4 does a complete circle, it is programed as 4 arcs all with the same center. Tools 5 & 6 are programed as 2 seperate arcs, with different center points. The machine stops between these arc moves when it should not. I checked I5183 it is set to 0 so there is no reason for it to stop blending.
at T4
N169 G2 X4.2 Y-2.1275 I-.7025 J0
N170 X3.4975 Y-1.425 I0 J.7025
Hesitation Very faint can not see but can feel in the part
N171 X4.2 Y-0.7225 I.7025 J0
N172 X4.9025 Y-1.425 I0 J-.7025
At T5
N219 G2 X5.1969 Y-1.425 I-.5601 J-.826
Blending stops here Visibly can see machine stop
N220 X4.7601 Y-2.205 I-.9969 J.046
I have attached the NC program that I am tring to run.
Thanks for any help. we would really like to solve this issue and put this project to bed.
Thanks
Anthony
M99 in main program not working
in PMAC NC PRO2
Posted
Hello All
I am trying to use an M99 P304 in my main NC program. In the manual it states that this should search for N304 and execute from this line on. It does not. It seems to perform a rewind to the top of the program and stop execution. There is no alarm. If I press cycle start the program starts from beginning. I looked in the Mill.m and found that there is no real code there execpt for a "Dwell0" and a note that says it looks like there is no code here there is and that it looks to make sure the subroutine has not been deleted. Any help would be greatly helpful.
Thanks
Anthony