bmccarney
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by bmccarney
-
-
I'm hoping for an explanation of how look ahead works in a Turbo PMAC2 (Brick Controller). We're controlling a rotator in either a 'Track' or 'Slew' mode with the code listed below. Segmentation is disabled and blending is on, so my impression is that Acceleration and Velocity I-variables would dictate the response regardless of the Ts value specified.
For a Slew move, P250 is updated once with the destination and we have found that the rotator will accelerate at the I217 rate to the max speed of i216, but then essentially abort and decelerate at I215 once it gets to the final position. Why? If this is a look ahead interference, what is it looking ahead to when only one destination is provided? Oddly enough, by disabling blending we've been able to get the move profile for Slews correct however Tracking behavior suffers. Does that make sense?
For Tracking moves, updated position information is provided at 2Hz which was then originally provided to the PMAC via P250 interpolated to 100Hz. We've found that over time the rotator seems to fall behind and our position error will grow. We've reproduced this issue on a benchtop setup, even when removing the interpolation and just providing the PMAC updates at 2Hz (InFreq is updated accordingly). We've experimented with specifying move times using Tm at 2Hz as well without success. What's odd is that the following error the PMAC reports makes it seem as though we're staying on target. Should it matter whether we set TM versus Ts? If a new position is arriving every 2Hz, should that dictate our TM/Ts settings? Our Tracking rates can vary pretty widely, from 10asec/sec up to 0.45deg/sec depending on elevation so we would like to have the smoothest response between updates (so in motion during the entire period as opposed to arriving at the destination and waiting).
////////////////////////////////
&2 ; define coordinate system 2
#2->10922.667X ; cts/deg
#define InFreq 100 ; Input Frequency [Hz]
Open prog 2 Clear
P253=1 ; indicate motion program running
DWELL 0
ABS
LIN
TA 0
TS (1000/(2*InFreq))
TM 0
P252=0
WHILE (P251=0) WAIT
WHILE (P251 > 0) ; do while we want to track
P252=P252+1
X(P250) ; move to position specified by P250
EndW
DWELL 0
P253=0 ; indicate motion program not running
Close
//////////////////////////////////////
Any assistance is appreciated, and please let me know if you need more information on the configuration. Don't assume I know what I'm talking about!
Thanks,
Ben
Help with look ahead
in Turbo PMAC
Posted