sanjay kumar katiyar
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by sanjay kumar katiyar
-
-
I tried to use a P variable to find out which block is running but it always shows 6 blocks ahead of actual block executing motion.
ie
P2000=1
x1 y1
P2000=2
x4 z8
P2000=3
x30 y30
-
In GeoBrick, without the use of GeoBrick drive setup utility the axis motor do not get moving. What parameters does this utility setup.
Can we setup motors without the use of GeoBrick setup application. What procedure is to be followed?
-
Does defining more M variables eats more PMAC time or the number of M variables doesn't matter.
Programmatically detect which and where a CS program is running
in Turbo PMAC
Posted
Thanks
it works well, but i have one problem that M var takes last value as 11 and never 12 in the program given below.
open prog 5
Clear
M4000==2
abs
M4000==3
linear
M4000==4
x500 z600F50
M4000==5
circle2
M4000==6
x300 z400 r1000
M4000==7
inc
M4000==8
linear
M4000==9
x300 y600 z300 F100
M4000==10
circle1
M4000==11
x200 y300 r500
M4000==12
Close