mitrekol
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by mitrekol
-
-
Ron, by now, you have either given up or resplved the problem. I have experience with PMAC on Entec winding machines and others as well. if you need further support feel free to contact me. tim@le-3.net
If you converted to PPMAC you would not need a rotary buffer as the available memory is so large. Your programs would then be loaded into a single buffered program file and run.
PPMAC Micro fsave and fload
in Power PMAC
Posted
I am attempting to implement the fsave and fload feature to save variables through a power cycle on a Micro PPMAC. Firmware version 2.2.1.3. My IDE version is IDE2_2_0-39.
This is a program conversion from TPMAC. To facilitate the coversion variable names have been assigned using the original Turbo I, P, M names as it provides a faster conversion.
Upon online commad "fsave" the following messages are reported through IDE:
fsave
Successful: FastSave using /var/ftp/usrflash/Project/Configuration/pp_custom_save.tpl
cp: cannot create regular file `/opt/ppmac/usrflash/Project/Configuration/pp_custom_save.cfg': Read-only file system
Fast Save Complete
Upone subsequent on-line issue of "fload" the following message is reported:
fload
Successful: FastLoad using /opt/ppmac/usrflash/Project/Configuration/pp_custom_save.cfg
The fsave command appears to have succeeded one time placing data in project folder Configuration\pp_custom_save.cfg which contains this information:
P89=58
P2161=0
P3005=3000
P3006=3000
P3007=2000
P3028=0.00400000019000000019
P3029=1
P3030=1.625
P3031=2.03999996185302734
P3032=-0.00999999977599999937
P3033=1.89600002769999998
P3034=0.620000004799999949
P3035=0.0790000036399999966
P3036=0.03125
P3037=0.0869600027800000036
.
.
.
and so on with all variables assigned from my pp_custom_save.tpl which is populated with this:
P89
P2161
P3005..3007
P3028..3040
P3501..3503
P3511..3513
P4126
P4156
P4161
P4162
P4501..4524
M2502
M702
I126
I226
I326
It appears as if the "fsave" worked once with this time stamp on the file
1/19/2017 3:26PM
then locked the file
`/opt/ppmac/usrflash/Project/Configuration/pp_custom_save.cfg': Read-only file
How can I resolve this?