JAN
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by JAN
-
-
HI,
i would like to know where and with which connector the TRUE DAC signals option on power brick lv are located?
in the analog IO connectors DB 15 HD X9-X12?
-
HI,
herafter the response to your queries:
IDE 2.2.0.39
Base card S/N:C000EBHH
mezzanine card S/N: C000CQ5W
terminal command responses:
vers
2.0.2.14
Gateio[0].PartNum
Gateio[0].PartOpt
Gateio[0].PartRev
Gateio[0].PartType
GateIo[0].PartNum=603603
GateIo[0].PartOpt=$1ff
GateIo[0].PartRev=6
GateIo[0].PartType=8
-
HI,
Im using a power pmac cpci format.
I would like to declare M variables that point to my IOs of the ACC11C opt1.
unfortunately the IDE didn't detect the option on this card.
hereafter an example:
M1098->Acc11C[_ACC11C_INDEX_].CtrlReg; configured to 15 (32 IN 16 OUT)
M1000->ACC11C[_ACC11C_INDEX_].DataReg[0].0.1; ACC11C In1(u.io:$A00000.8.1 )
now the only method that i found to point to the first input of the option card
is
M1033->u.io:$A00000.16.1 ;
question: is there a trick to declare M1033 as I did for M1000 ?
TRUE DAC on Power brick LV
in Power PMAC
Posted
HI,
i would like to know where and with which connector the TRUE DAC signals option on power brick lv are located?
in the analog IO connectors DB 15 HD X9-X12?