bbay
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by bbay
-
-
Hello!
Does anyone have experience using a touch probe to capture machine position?
I have a Renishaw OMP400, OMM-2, and OSI wired to a Power PMAC through the ACC65E digital I/O card.
I intend for the PMAC to record position, halt motion, and move back upon probe trigger.
My attempts to use "software capture" triggered moves (e.g. X50^-50) have failed, likely because it was misread as overtravel.
Is there a way to use hardware/software capture without disabling overtravel protection? Might it be simpler, albeit less accurate, to implement manually through a PLC? E.g. a while loop that checks for the triggered input.
The machine is a 3-axis parallel manipulator (tri-pyramid robot).
My current procedure runs a plc with the following for each motor:
Motor[ii].pCaptFlag = ACC65E… // Capture when probe triggers
Motor[ii].CaptFlagBit = 2 // Probe bit
Motor[ii].captureMode = 1; // Software capture, input triggering
Motor[ii].RapidSpeedSel = 0; // Peak velocity is now Motor[x].JogSpeed
Motor[ii].JogSpeed = very low // Speed at which probe will approach part
and
Touch probe (capturing machine position)
in Power PMAC
Posted
Hello!
Does anyone have experience using a touch probe to capture machine position?
I have a Renishaw OMP400, OMM-2, and OSI wired to a Power PMAC through the ACC65E digital I/O card.
I intend for the PMAC to record position, halt motion, and move back upon probe trigger.
My attempts to use "software capture" triggered moves (e.g. X50^-50) have failed, likely because it was misread as overtravel.
Is there a way to use hardware/software capture without disabling overtravel protection? Might it be simpler, albeit less accurate, to implement manually through a PLC? E.g. a while loop that checks for the triggered input.
The machine is a 3-axis parallel manipulator (tri-pyramid robot).
My current procedure runs a plc with the following for each motor, before executing the rapid trigger move:
Motor[ii].pCaptFlag = ACC65E… // Capture when probe triggers
Motor[ii].CaptFlagBit = 2 // Probe bit
Motor[ii].captureMode = 1; // Software capture, input triggering
Motor[ii].RapidSpeedSel = 0; // Peak velocity is now Motor[x].JogSpeed
Motor[ii].JogSpeed = very low // Speed at which probe will approach part