I have written many HMI's that use DPRam and the BinRot to download millions of lines of NC code... actually running programs for weeks at a time on a single machine.
I have a good example application showing basics of doing this both with ASCII and Binary type buffer.
But it is written in Visual Studio and using PcommServer
If this will help you I be glad to give you a full copy with source.
-I have attached a pdf that describes this demo app...
Are you connected to PMAC with USB or Ethernet ?
Can you show me the line of code actually sending the line to execute to the buffer ?
I'm confused reading all the posts above... and not sure what is or is not working ?
Can you describe simply what IS and what IS NOT working ?
I also have some examples of using PMAC Interrupts and data gathering techniques.
Note that with my NC hmi I use multiple threads, one to send the data to the pmac buffer, and a different thread to update the HMI to watch motor positions, status, NC line number executing, and even draw on simple 2D graphics the motion as it is executing...
Thanks,
mike
Hello,
I using the DPRAM binary ROT recently,but I don't complete the function of this.There is a problem that bothers me.When I down load the file to the DPRAM ROT,then the PMAC will get the file text from the DPRAM ROT to the internal ROT .The file awalys down load to the DPRAM ROT completely .But there are awalys some file don't down load into ROT in the PMAC.Maybe I don't understand the mechanism of the DPRAM Binary ROT and ROT.and I can't down load the PDF file for your privided. Can you give me the documents about this .
Use Rotary Buffer & update the Coordinates
in Turbo PMAC
Posted
Hello,
I using the DPRAM binary ROT recently,but I don't complete the function of this.There is a problem that bothers me.When I down load the file to the DPRAM ROT,then the PMAC will get the file text from the DPRAM ROT to the internal ROT .The file awalys down load to the DPRAM ROT completely .But there are awalys some file don't down load into ROT in the PMAC.Maybe I don't understand the mechanism of the DPRAM Binary ROT and ROT.and I can't down load the PDF file for your privided. Can you give me the documents about this .
Thanks