Jump to content
OMRON Forums

GeoBrick LV Setup program Issue


GSS

Recommended Posts

Motor set up goes fine, step two goes fine, enter the voltage test and it say's 100% complete but cannot continue or implement gains and then test times out.  All 8 axes respond the same.

Any help ?

Link to comment
Share on other sites

  • Replies 6
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

To be more clear, the motor details step 1 go fine, Step 2 defining the encoder counts goes fine, step 3 which is the voltage test says 100% complete, the motor does 6-7 moves, but I cannot continue like I could in Geo Brick setup.

I cannot step forward to the phasing step for completion.

Link to comment
Share on other sites

Let me know what link you were looking for, I’m sure I can find it.

The software should provide a response to any failed steps with a suggested corrective action. Note that this is very obsolete hardware and software and as such TSG does not have any working systems to do simulations.

But as I previously mentioned, the manual at the link contains downloadable code samples for “complete” setup that has been well tested for any errors. You can copy and paste these into the editor of Pewin32pro2 as a “configuration” file for download. Some of the code examples need specific information pertaining to your actual hardware. When information is required, a commentary ending with “–User Input” is inserted, as in the following code snippet:

#define DCBusInput 60  ; DC Bus Voltage -User Input
#define Mtr1Voltage 24 ; Motor 1 Rated Voltage [VDC]-User Input
#define Mtr2Voltage 24 ; Motor 2 Rated Voltage [VDC]-User Input
#define Mtr3Voltage 24 ; Motor 3 Rated Voltage [VDC]-User Input
#define Mtr4Voltage 24 ; Motor 4 Rated Voltage [VDC]-User Input

 

I would suggest starting from a factory reset condition:

$$$***
Save
$$$

 

Link to comment
Share on other sites

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...