GSS Posted Thursday at 07:01 PM Share Posted Thursday at 07:01 PM Backplane HW: ACC-E1 Power Supply 3x0-603766 Turbo PMAC2 CPU ACC-24E2 4 axis Interface External HW: Geo Drive Direct PWM MCG Motor PN 3483-ME3921 4 A Continuous Current 8 poles 1.6 ohms pase to phase 36 V nominal Drive thermals are disabled via jumpers Encoder from moter is utilizing A, B & C and U, V & W. Have that connector wired to 12 Pin to ACC-24E2 Manual says I can use 110 VAC input to Geo Drive which I have. Motor has worked on several Geo drives and I have 3 of them and all have same problem. Followed manuals cover to cover. This setup should work but I'm getting Fault code 2 on the single axis I'm testing which is Over Current. Question's : Can I get PN and quote for 36 pin mating connector from ACC-24E2 to the Geo Drive Direct PWM ? Can I get PN and quote for 15-Pin Female D-Shell to 12 Pin Phoenix Connector for the encoder which would include the Hall effect wiring as well ? I have followed all drawings in the manuals and, yet again, failure mode !! Quote Link to comment Share on other sites More sharing options...
steve.milici Posted Thursday at 08:08 PM Share Posted Thursday at 08:08 PM We would need more details on how configuration was achieved to better comment, but if this motor and feedback worked on other Geo Direct PWM drives It could be that the three drives with the over current issue may have compromised electronics in the current feedback circuits and will require repair. You will need to provide “from” and “to” details on the “15-Pin Female D-Shell to 12 Pin Phoenix Connector” as there is no Omron part that fits this description. Here are the order PNs with list prices for compatible Geo Direct PWM to ACC-24E2 cables: 36in CK3WCAAD009A $382.00 72in CK3WCAAD018A $409.00 144in CK3WCAAD036A $488.00 Contact your local Omron distributor for a price and delivery quote. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted Thursday at 10:10 PM Share Posted Thursday at 10:10 PM Contact me directly at ODT-Support@Omron.com. I “understand” better what you are working on now. The “15-Pin Female D-Shell to 12 Pin Phoenix Connector” is to “cross” an encoder connection for an ACC-24E2A to an encoder connection for an ACC-24E2. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.