shansen Posted June 25, 2011 Share Posted June 25, 2011 Is there a way that I can delete files/folders that I am not using in the IDE? For example, in one project all of my code is under the 'C Language\Realtime Routines' folder. Is there a way to delete the 'Background Programs' and 'CPLCs' folders for clarity? I realize that the PPmac expects a well defined folder structure, but is there a way to hide these unused folders in the IDE? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted June 27, 2011 Share Posted June 27, 2011 Is there a way that I can delete files/folders that I am not using in the IDE? For example, in one project all of my code is under the 'C Language\Realtime Routines' folder. Is there a way to delete the 'Background Programs' and 'CPLCs' folders for clarity? I realize that the PPmac expects a well defined folder structure, but is there a way to hide these unused folders in the IDE? Hi, At this point NO! This is our default project template. But I will take this as input and I will see if we can do anything in the future IDE . Thanks, Atul Link to comment Share on other sites More sharing options...
KEJR Posted June 28, 2011 Share Posted June 28, 2011 +1 Although I don't have a *big* problem with this, it would be slick if we could do that at some time in the future. We will be using only a small subset of the project tree for any given machine. KEJR Link to comment Share on other sites More sharing options...
Recommended Posts