grlarkin Posted October 24, 2012 Share Posted October 24, 2012 I have a LabVIEW application running on Windows that communicates with a Turbo PMAC chassis. There is some interest in porting the application to a real-time platform, either a PXI crate which would run a PharLap kernal or a compactRIO chassis that would run vxWorks. Is there any documentation on how to talk to Turbo PMAC directly over Ethernet using raw TCP/IP? Glenn Larkin Lawrence Livermore National Labs Link to comment Share on other sites More sharing options...
Dan1223 Posted October 25, 2012 Share Posted October 25, 2012 Check the Turbo PMAC Users Manual. There is a section Turbo PMAC Ethernet Protocol Link to comment Share on other sites More sharing options...
Sina.Sattari Posted October 25, 2012 Share Posted October 25, 2012 In addition to Dan1223's suggestion, there is also an open source communication library which was developed for Linux which can be useful as a guide. Please see the following post: http://forums.deltatau.com/showthread.php?tid=57 Link to comment Share on other sites More sharing options...
grlarkin Posted October 25, 2012 Author Share Posted October 25, 2012 I downloaded the Linux example code yesterday and have just started looking at it. The section in the Turbo PMAC manual is exactly the documentation I was hoping to find. Thanks so much. Link to comment Share on other sites More sharing options...
Recommended Posts