aims Posted May 14, 2015 Share Posted May 14, 2015 Hi, I have power clipper connect with servo motor. So how i can get motor information and put into the power clipper? Link to comment Share on other sites More sharing options...
steve.milici Posted May 14, 2015 Share Posted May 14, 2015 The manual for the Power Clipper can be found in the Forum's FileDepot at: http://forums.deltatau.com/filedepot/download.php?f=Power%20PMAC/Manuals/Hardware%20Reference%20Manual/Power%20PMAC%20Clipper%20HRM%20preliminary.pdf [FILE REMOVED] Link to comment Share on other sites More sharing options...
aims Posted May 15, 2015 Author Share Posted May 15, 2015 Where can i get the information of the amplifier, motor and so on to do the setup to Power Clipper? Link to comment Share on other sites More sharing options...
aims Posted May 15, 2015 Author Share Posted May 15, 2015 Just like the picture that attached. How to manufacturer since the selection only have "Add New...."? Link to comment Share on other sites More sharing options...
Alex Anikstein Posted May 15, 2015 Share Posted May 15, 2015 That information is usually on a datasheet provided by the manufacturer of the servo motor or drive. If you input the information, you can then select "Add to Database" on the right side to add it to your database if you have that same motor in other locations. Link to comment Share on other sites More sharing options...
aims Posted May 19, 2015 Author Share Posted May 19, 2015 Hi, the motor feedback type i using is incremental encoder. But I found that there is no incremental encoder in the system setup> motor setup feedback type selection. So what I need to select? Link to comment Share on other sites More sharing options...
Alex Anikstein Posted May 19, 2015 Share Posted May 19, 2015 The Motor Feedback Type selection is asking what type of incremental/absolute encoder it is. For instance, Quadrature is one common type of incremental encoder, but is not the only one, so you would need to consult the data sheet for your encoder to see what protocol/type of incremental encoder it is. You may be able to guess from the pinout of the encoder, too (Sine and Cosine could be a Sinusoidal Encoder, while A and B channels may be Quadrature), though multiple protocols may use the same signal names, so this is not as reliable. For questions like these, we do strongly recommend attending our training course if it is possible, though I see from your other post that you are at least looking through the slides. Link to comment Share on other sites More sharing options...
aims Posted May 20, 2015 Author Share Posted May 20, 2015 Thanks for your info. After do this setup, so motor setup is done? I wish to use power clipper send pulse to drive my servo motor. So the driver which drive the servo motor is consider amplifier? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted May 20, 2015 Share Posted May 20, 2015 Yes. Link to comment Share on other sites More sharing options...
Recommended Posts