DaveBarnett Posted December 14, 2015 Share Posted December 14, 2015 'Looking to use PowerClipper board inside an industrial control box. But, DT doesn't seem to offer a suitable enclosure for the Clipper. Any thoughts? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted December 14, 2015 Share Posted December 14, 2015 A 4-Axis Power Brick Controller with 12-bit filtered PWM outputs provides essentially the same functionality as a Power Clipper, except it is enclosed. Delta Tau China also sells an enclosed Turbo Clipper called the IMAC (i.e. if you want to go international): http://deltatau-china.com/html/xt/2449.html Link to comment Share on other sites More sharing options...
iannicholson Posted September 25, 2017 Share Posted September 25, 2017 We are looking to have an enclosure custom-designed for the Clipper. Does Delta Tau sell the IMAC or anything similar in the US at this point? We are using Turbo Clipper and have not yet moved to Power Clipper. Link to comment Share on other sites More sharing options...
Richard Naddaf Posted September 26, 2017 Share Posted September 26, 2017 No plans to make an enclosure for the Power Clipper. This is an integrator - end user project. The Power Clipper is intended to be an integrated solution using the long pins option. The only similar enclosed solution is the Power Brick Controller as insider mentioned. Link to comment Share on other sites More sharing options...
Recommended Posts