hjpark Posted December 5, 2019 Share Posted December 5, 2019 Hi, There is a problem with install IDE 4.3.x.x I see the message 'Failed to install the PowerPMAC IDE Version Selector' IDE 4.2.x.x and 3.1.x.x can be installed. Do I have to delete any file or registry or any existing program? Link to comment Share on other sites More sharing options...
Omron Forums Support Posted December 5, 2019 Share Posted December 5, 2019 What IDE version is being installed? Is this with the patch or the full installer? What versions are already installed? If you are trying to install 4.3.2.19 with the patch, that would be installed on top of IDE 4.3.0.107. If you are using a full installer and not a patch, IDE 4 should be removed before installing. Link to comment Share on other sites More sharing options...
hjpark Posted December 6, 2019 Author Share Posted December 6, 2019 No IDE is installed. I deleted all IDE before installation. That message is appeared in 4.3.0.107, 4.3.2.19 both (full installer, downloaded at 'www.deltatau.com') No problem on other PCs. Is there any way other than formatting the disk? Link to comment Share on other sites More sharing options...
hjpark Posted December 11, 2019 Author Share Posted December 11, 2019 What IDE version is being installed? Is this with the patch or the full installer? What versions are already installed? If you are trying to install 4.3.2.19 with the patch, that would be installed on top of IDE 4.3.0.107. If you are using a full installer and not a patch, IDE 4 should be removed before installing. No IDE is installed. I deleted all IDE before installation. That message is appeared in 4.3.0.107, 4.3.2.19 both (full installer, downloaded at 'www.deltatau.com') Please refer to the attachmentPMAC_Installer.txt Link to comment Share on other sites More sharing options...
hjpark Posted December 11, 2019 Author Share Posted December 11, 2019 This problem was solved! 1. When the massage is appeared, don't click 'OK' 2. You can see the Version selector installer is created in "C:\Users\{User name}\AppData\Local\Temp\{34C44C9A-0A6B-42F2-B2FF-D88F1155F907}" 3. Copy this folder to any path 4. Excute "VersionSelector.msi" Link to comment Share on other sites More sharing options...
Recommended Posts