Thank you for reply.
"0.1um per pulse" means "0.025um per count", when Gate3.Chan[j].Encctrl is set 3 or 7
To ask again, how do you calculate max speed of quadrature encoder with ACC-24E3?
Is it related to Gate3.EncClockDiv? or line reciever's maximum operating frequency?
If it is related to line reciever, what is the maximum operating frequency?
First of all, thank you for your help.
I'm reviewing quadrature encoder specifications.
As i know, line receiver specification is 10MHz.
So, when I use quadrature encoder of 0.1 micrometer per pulse, I can use 4m/s at max speed.
Is that correct?
This problem was solved!
1. When the massage is appeared, don't click 'OK'
2. You can see the Version selector installer is created in "C:\Users\{User name}\AppData\Local\Temp\{34C44C9A-0A6B-42F2-B2FF-D88F1155F907}"
3. Copy this folder to any path
4. Excute "VersionSelector.msi"
No IDE is installed.
I deleted all IDE before installation.
That message is appeared in 4.3.0.107, 4.3.2.19 both (full installer, downloaded at 'www.deltatau.com')
Please refer to the attachment PMAC_Installer.txt
No IDE is installed.
I deleted all IDE before installation.
That message is appeared in 4.3.0.107, 4.3.2.19 both (full installer, downloaded at 'www.deltatau.com')
No problem on other PCs.
Is there any way other than formatting the disk?
Hi,
There is a problem with install IDE 4.3.x.x
I see the message 'Failed to install the PowerPMAC IDE Version Selector'
IDE 4.2.x.x and 3.1.x.x can be installed.
Do I have to delete any file or registry or any existing program?