Hello.
I have some problem with the acceleration in linear mode.
Actually it is more correct that the problem is 'Jerk'.
When i tried a simple motion program which is set with 'TA 400' and 'TS 0', i expected that the total acceleration time will be 400ms. But it didn't work , it derived 420ms in plots for 'velocity- time'.
So i tried the motion program with another value for TA and TS. It wasn't changed with having an interval, 20ms. (if i test it with Ta 500 and TS 0, the total acceleration time is resulted in 520ms.
And then i saw an reduction trend for 20ms when the acceleration value went to 'zero' in the plots for 'acceleration-time'. i just expected the acceleration value went to 'zero' ,just like a pulse without any reduction trend or decreasing trend.
Why didn't it work as what i expect? i searched some initial value for acceleration , jerk or speed in coordinate system for motion program. But i couldn't catch anything.
So, i'm looking for answers.
Thank you reading my question.