kst774
-
Posts
3 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by kst774
-
-
Motor[*].InvJmax parameter will limit jerk magnitude regardless of your motion program requests.
This parameter's default value is 20 motor units/sec^2
Perhaps this is what you are seeing.
Thank you for your answer.
I already tried to include the parameter, which is '0.0000001'.
In addition 'Motor[*].InvAmax' and 'Motor[*].InvDmax is also included in the motion prog.
But there isn't any change. :-(
I got it from my coworker. It comes out from servo-cycle. For gathering on servo-cycle(1ms), the plot is gathered with 2 servo-cycle(2ms).
So i get the reduction trend from the plot as 2ms(sorry , it wasn't 20ms).
Thank you :-)
-
Hello.
I have some problem with the acceleration in linear mode.
Actually it is more correct that the problem is 'Jerk'.
When i tried a simple motion program which is set with 'TA 400' and 'TS 0', i expected that the total acceleration time will be 400ms. But it didn't work , it derived 420ms in plots for 'velocity- time'.
So i tried the motion program with another value for TA and TS. It wasn't changed with having an interval, 20ms. (if i test it with Ta 500 and TS 0, the total acceleration time is resulted in 520ms.
And then i saw an reduction trend for 20ms when the acceleration value went to 'zero' in the plots for 'acceleration-time'. i just expected the acceleration value went to 'zero' ,just like a pulse without any reduction trend or decreasing trend.
Why didn't it work as what i expect? i searched some initial value for acceleration , jerk or speed in coordinate system for motion program. But i couldn't catch anything.
So, i'm looking for answers.
Thank you reading my question.
Some problem with the acceleration in linear mode
in Power PMAC
Posted
Thank you for your answer.
Hm.. I knew that i tried the result in non-segmentation mode(coord[].segmovetime=0, linear mode).
Any way, if i have a problem just like the result again, i would solve it from your answer :-).
Thank you. Have a nice day~!