jnasri
-
Posts
6 -
Joined
-
Last visited
-
Days Won
1
Content Type
Profiles
Forums
Events
Downloads
Posts posted by jnasri
-
-
I added MacroinitPLC and changed the PowerBrick[0].MacroEnableA value to $0BFFFF00 on the slave
but the following command that i use in one of my PLCs didnt repond : macro timeout
MacroAuxiliaryRead 0,P555, P556
it responds only if the PowerBrick[0].MacroEnableA = $0FFFFF00 OR PowerBrick[0].MacroEnableA = $0FBFFF00
I added a ctr to see in how much time the active status is reached and it is about 30 second +/- 20 seconds
i added also a ctr to see in how mush time the MacroAuxiliaryRead Command is successfull and the result is 5 to 30 retry ( 1 second between each command)
do you have an explanation for that?
-
I tried your suggestion : "PowerBrick[0].MacroModeA =$808000 on the Slave".
unfortunately it doesn't change the activation pb on power on of the master side.
on power on:
slave side: i have auxslaveconfigfault ( see Slavestatus2.png)
PowerBrick[0].MacroModeA =$808200
on the master side: see MasterStatus2.PNG
note: the macro status leds are green on both sides ( master and slave).
-
Hi all,
I am having some trouble with the Macroactivation on power on of a Brick LV:
The hardware setting is as follow: 1 Powerbrick LV as Master & 1 Powerbrick LV as Slave.
the config of the Master
PowerBrick[0].MacroModeA =$00403000;
PowerBrick[0].MacroModeB =$00000000;
PowerBrick[0].MacroEnableA =$0FFFFF00;
PowerBrick[0].MacroEnableB =$0;
PowerBrick[1].MacroModeA =$0;
PowerBrick[1].MacroModeB =$0;
PowerBrick[1].MacroEnableA =$0;
PowerBrick[1].MacroEnableB =$0;
Macro.TestPeriod =10/Sys.ServoPeriod;
Macro.TestMaxErrors =Macro.TestPeriod/10;
Macro.TestReqdSynchs =Macro.TestPeriod-Macro.TestMaxErrors;
Macro.IOTimeout =0;
config of the slave
PowerBrick[0].MacroModeA =$00408000;
PowerBrick[0].MacroModeB =$0;
PowerBrick[0].MacroEnableA =$0FFFFF00;
PowerBrick[0].MacroEnableB =$0;
PowerBrick[1].MacroModeA =$0;
PowerBrick[1].MacroModeB =$0;
PowerBrick[1].MacroEnableA =$0;
PowerBrick[1].MacroEnableB =$0;
Macro.TestPeriod = 10/Sys.ServoPeriod;
Macro.TestMaxErrors = Macro.TestPeriod/10;
Macro.TestReqdSynchs = Macro.TestPeriod-Macro.TestMaxErrors;
Randomly on power on , the master macro status never pass to Active.
I have the following macro status:
on the On master:
Macro.status[0].active=0
Macro.Status[0].SynchMaster =1
Macro.Status[0].TestEnabled=0
On the slave:
Macro.status[0].active=1
Macro.Status[0].SynchMaster =0
Macro.Status[0].TestEnabled=1
From the master side, I issued some line command as follow:
Macro.RingTest[0].PwrOnErrCntr
Macro.RingTest[0].PwrOnErrCntr=0
Macro.Status[0].RingError
Macro.Status[0].RingError=0
Macro.Status[0].ErrorsFault
Macro.Status[0].ErrorsFault=0
clrf
stdin:6:5: error #50: MACRO COM TIMEOUT: clrf
Macro.RingTest[0]
stdin:7:2: error #20: ILLEGAL CMD: Macro.RingTest[0]
Macro.Rings
Macro.Rings=1
Macro.ICs
Macro.ICs=4
Macro.IC3s
Macro.IC3s=2
Ldata.CmdStatus
Ldata.CmdStatus=0
Macro.RingTest[0].RingBrkStationNum
Macro.RingTest[0].RingBrkStationNum=0
MacroControllerDetect
Error: PowerBrick[0] isn't in a connected Ring
Error: PowerBrick[1] isn't in a connected Ring
MacroControllerDetect
Error: PowerBrick[0] isn't in a connected Ring
Error: PowerBrick[1] isn't in a connected Ring
When I disconnect/ reconnect the fiber optics With the brick lv powered on the status of the macro change to active.
Please help me to diagnose the problem.
Best regards
-
There is a known issue where if you change a gain and don't click out of the box before running the tuning move, the window has a small chance of crashing. Do you think this could be your issue?
I know some changes to the tune tool are coming that will address this issue.
Thank you for your reply. I am not sure that it is the case. I will follow your instruction on clicking outside the box and make you informed if it does stop crashing.
-
Hi everebody,
I am using power pmac IDE 43.2.19 with powerbrick LV (CPU:PowerPC,460EX / frimware 2.3..2.5) on a windows 10 Pro 64 bit.
I have a problem with the Tuning tool which get stuck after 5 to 10 successfull sine or trapezoidal or even step curves profile generation.
it is impossible to exit neither tune tool nor the IDE itself when it get stuck. i have to stop it via the windows task manager.
the problem is occuring every time i launch the tune tool.
please help!
Phase/Servo/RTI errors when opening or closing IDE (Quad core)
in Power PMAC
Posted
Hello,
We are facing the same sort of problem from our side as well.
Do you have an update or a fix that can be deployed?
best regards