Jump to content
OMRON Forums

jnasri

Members
  • Posts

    6
  • Joined

  • Last visited

  • Days Won

    1

Everything posted by jnasri

  1. Hello, We are facing the same sort of problem from our side as well. Do you have an update or a fix that can be deployed? best regards
  2. I added MacroinitPLC and changed the PowerBrick[0].MacroEnableA value to $0BFFFF00 on the slave but the following command that i use in one of my PLCs didnt repond : macro timeout MacroAuxiliaryRead 0,P555, P556 it responds only if the PowerBrick[0].MacroEnableA = $0FFFFF00 OR PowerBrick[0].MacroEnableA = $0FBFFF00 I added a ctr to see in how much time the active status is reached and it is about 30 second +/- 20 seconds i added also a ctr to see in how mush time the MacroAuxiliaryRead Command is successfull and the result is 5 to 30 retry ( 1 second between each command) do you have an explanation for that?
  3. I tried your suggestion : "PowerBrick[0].MacroModeA =$808000 on the Slave". unfortunately it doesn't change the activation pb on power on of the master side. on power on: slave side: i have auxslaveconfigfault ( see Slavestatus2.png) PowerBrick[0].MacroModeA =$808200 on the master side: see MasterStatus2.PNG note: the macro status leds are green on both sides ( master and slave).
  4. Hi all, I am having some trouble with the Macroactivation on power on of a Brick LV: The hardware setting is as follow: 1 Powerbrick LV as Master & 1 Powerbrick LV as Slave. the config of the Master PowerBrick[0].MacroModeA =$00403000; PowerBrick[0].MacroModeB =$00000000; PowerBrick[0].MacroEnableA =$0FFFFF00; PowerBrick[0].MacroEnableB =$0; PowerBrick[1].MacroModeA =$0; PowerBrick[1].MacroModeB =$0; PowerBrick[1].MacroEnableA =$0; PowerBrick[1].MacroEnableB =$0; Macro.TestPeriod =10/Sys.ServoPeriod; Macro.TestMaxErrors =Macro.TestPeriod/10; Macro.TestReqdSynchs =Macro.TestPeriod-Macro.TestMaxErrors; Macro.IOTimeout =0; config of the slave PowerBrick[0].MacroModeA =$00408000; PowerBrick[0].MacroModeB =$0; PowerBrick[0].MacroEnableA =$0FFFFF00; PowerBrick[0].MacroEnableB =$0; PowerBrick[1].MacroModeA =$0; PowerBrick[1].MacroModeB =$0; PowerBrick[1].MacroEnableA =$0; PowerBrick[1].MacroEnableB =$0; Macro.TestPeriod = 10/Sys.ServoPeriod; Macro.TestMaxErrors = Macro.TestPeriod/10; Macro.TestReqdSynchs = Macro.TestPeriod-Macro.TestMaxErrors; Randomly on power on , the master macro status never pass to Active. I have the following macro status: on the On master: Macro.status[0].active=0 Macro.Status[0].SynchMaster =1 Macro.Status[0].TestEnabled=0 On the slave: Macro.status[0].active=1 Macro.Status[0].SynchMaster =0 Macro.Status[0].TestEnabled=1 From the master side, I issued some line command as follow: Macro.RingTest[0].PwrOnErrCntr Macro.RingTest[0].PwrOnErrCntr=0 Macro.Status[0].RingError Macro.Status[0].RingError=0 Macro.Status[0].ErrorsFault Macro.Status[0].ErrorsFault=0 clrf stdin:6:5: error #50: MACRO COM TIMEOUT: clrf Macro.RingTest[0] stdin:7:2: error #20: ILLEGAL CMD: Macro.RingTest[0] Macro.Rings Macro.Rings=1 Macro.ICs Macro.ICs=4 Macro.IC3s Macro.IC3s=2 Ldata.CmdStatus Ldata.CmdStatus=0 Macro.RingTest[0].RingBrkStationNum Macro.RingTest[0].RingBrkStationNum=0 MacroControllerDetect Error: PowerBrick[0] isn't in a connected Ring Error: PowerBrick[1] isn't in a connected Ring MacroControllerDetect Error: PowerBrick[0] isn't in a connected Ring Error: PowerBrick[1] isn't in a connected Ring When I disconnect/ reconnect the fiber optics With the brick lv powered on the status of the macro change to active. Please help me to diagnose the problem. Best regards
  5. Thank you for your reply. I am not sure that it is the case. I will follow your instruction on clicking outside the box and make you informed if it does stop crashing.
  6. Hi everebody, I am using power pmac IDE 43.2.19 with powerbrick LV (CPU:PowerPC,460EX / frimware 2.3..2.5) on a windows 10 Pro 64 bit. I have a problem with the Tuning tool which get stuck after 5 to 10 successfull sine or trapezoidal or even step curves profile generation. it is impossible to exit neither tune tool nor the IDE itself when it get stuck. i have to stop it via the windows task manager. the problem is occuring every time i launch the tune tool. please help!
×
×
  • Create New...