Jump to content
OMRON Forums

Sam01

Members
  • Posts

    12
  • Joined

  • Last visited

Everything posted by Sam01

  1. Hello everyone, I tried running a G code on my PMAC and I noticed that Rapid move (G00) and Dwell (G04) commands are not responding the way I thought they should considering their corresponding PMAC program command. The G04 does not respond and the G00 command moves very slow than expected I have run the G-code subroutine program (PROG 1000). It seems strange to me because other G-code commands work alright. Please can anyone provide any information that will guide me to fix this? Thank you Regards, Sam
  2. Sam01

    program error

    Thank you AAnikstein for your response. Like you advise the coordinate system segmentation was zero. The problem has been fixed.
  3. Sam01

    program error

    Hello everyone, Please I want to ask if it is possible for the turbo PMAC to not respond to certain commands. I noticed that my machine doesn't respond to certain commands such as CIRCLE 1 and CIRCLE 2. When I issue these commands the machine executes them as a straight (LINEAR) command. Also, I changed the plain but I didn't notice any changes. that is I used K-1 at first then later changed it to J-1 and I-1 but didn't notice any changes. I also wrote a program using ABS and later changed to INC yet I didn't notice any changes in the execution. Is it possible that the machine doesn't respond to certain commands or what could be the cause ? Please I will appreciate your contribution' Thanking you in advance. Best Regards, Samuel
  4. Sam01

    program error

    Hello everyone, I just configured a micro milling machine and in order to test the machine, I wrote a simple program to generate a profile. The program has linear and circle commands. I ran the program yesterday and it worked. it generated the profile I wanted. but I came in today to test the same program but it's not generating the profile. instead of circular motion, it is generating a straight line. please can anybody tell me what might be the cause? I will sincerely appreciate your assistance to help me fix this problem Thank you Regards, Samuel
  5. Hello everyone, Please I want to ask if it is possible to run a Profile Simulation using the PEWIN32PRO2 software? I am setting up a micro-milling system that will cut simple and complex profiles. So, I want to write a program that can cut a profile using the micro milling machine but before conducting a real cutting process, I want to run the program and see the resulting output profile on the terminal. Please I will like to know if this is possible using the PENWIN32PRO2 SOFTWARE? Thank you. Regards, Sam PS: I using three motors with a TURBO2, X4, and a spindle.
  6. Thank you so much Gregs and Eric. The problem has been solved. I cleared the settings using the $$$*** command and I uploaded the setup again. When I did that it worked fine as expected and all the phasing and home of the motors were completed without errors. Thank you. meanwhile, my PMAc is a TURBO2, X4 Sam
  7. Hello everyone, Please can some educate me on how to fix Fatal following Error and warning following Error? I always get Fatal following Error and Warning following Error on motor 3 whenever I attempt homing and phasing. I have three motors and motors 1 and 2 usually complete homing and phasing except motor 3. Please can someone tell me how I can fix it? Thank you. Sam.
  8. Sam01

    Geo Brick LV

    Thank you so much for the information.
  9. Dear Gregs, Thank you for the information. I just got to know that my machine is a QMAC Turbo- TURBO2, X4, Version 1.947 after I entered TYPE and VERSION on the PEWIN32PRO terminal. I have been making a lot of attempts to set up the Geo brick amplifier and controller and I have not succeeded so I wanted to use PMAC IDE because I thought the difficulty I was facing was a result of using PEWIN32PRO. Thank you for letting me know that the IDE cannot work with my machine since it's a TURBO. Regards, Samuel
  10. Dear Sir, I am using a Windows 10 OS. I have installed Power PMAC IDE (Ver 4.4.1.7). I am having issues with establishing communication. Please I solicit your kind assistance. Kindly reply at the earliest... Thank you
  11. Sam01

    Geo Brick LV

    Hello everyone, I just started using the Geo Brick LV amplifier/controller. Please can anyone give me the manual for the Geo Brick LV setup software? Thank you.
×
×
  • Create New...