OK do I need remove card from pci slot and provide separate power to the card then connect to an open com port via rs-232? or just leave it in PCI slot and set up a com port that way. Please understand that this is my first foray into older style pmacs
I have a similar issue, in that the PCI card is not detected, so you are saying that serial connection is the option to use if the device is not detected via PCI slot?