msilverman
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by msilverman
-
-
We require the USB configuration due to consistent issues with vital steps missed through the IDE, so having a thumbdrive to eliminate human error seems necessary at this point.
Currently loading onto a PowerBrick from USB drive. It seems to be loading the project itself fine, I have checked in the PMAC files (both through ftp and uploading the code from the PMAC after the thumbdrive upload) and it appears identical to the expected project.
Unfortunately, every time the IDE is open it gives the project load error. When attempting to run the uploaded code that was on the PMAC, it results in an error involving the capp.out file.
I have tried both methods mentioned here:
And it always results in the same error:
How can I troubleshoot these errors/prevent them in the future when configuring with the USB?
-
When trying to build our project it seems as though our current set up gets overwritten by this systemsetup.cfg file, with different values than what we've specified, despite not selecting this file to download with the config file download process.
It appears to be overwriting this value (and others) from our file.
We are just trying to understand the purpose of systemsetup.cfg, if we can work with it and specify values within it, or if there is a possible work around.
-
I've recently upgraded to IDE 4, and have been unable to load my project solution files, despite accepting the file upgrade.
The errors I've received are:
Error - value cannot be null, parameter name: url
The option to use new PDO mapping name has been set to false because this project may have a program that uses existing name format. Please change the option on the property of the project to use the new format.
When I try to go to the property settings of the project within the IDE, it says there are no properties.
Any idea what this is trying to have me do and how to work around it?
Downloading Configuration From USB Drive
in Power PMAC
Posted · Edited by msilverman
Removed accidental image upload at end to avoid confusion
With the desired setup built and downloaded, config files downloaded, I've then connected to the PMAC to access the usrflash folder.
From there, I copy the contents into my own flashdrive in a PowerPMAC folder, as the steps in the linked forum post instruct.
To make sure that the PMAC begins in a factory reset state, I issue the '$$$***' command, power off, eject then add the programmed USB, then power on again.
This is where the ProjectLoadErr and PwrOnFault occur, after turning on power with the USB in the PMAC and connecting to the IDE.
In order to see what the flash has programmed the PMAC with, I upload the project from the PMAC.
From here, I will try both building and downloading the project that appears to have been loaded into the IDE, then factory resetting, and opening the archive it has made of the PMAC code and building and downloading that project as well.
(The message that gave me the impression that the project was loaded and opened in the IDE:
)
On attempting to build and download all programs from the code that was opened from the PMAC, this is the message that I receive.
I will then double check by sending the factory reset command.
Next, I will clear the current solution, then open the program in the IDE from the archive that was created earlier.
Now that the PMAC has no program, the old program that was archived is open in the IDE, I now attempt to build and download, which results in the exact same error.