PMAC Technology FAQ
Frequently Asked Questions about PMAC Technology.
27 topics in this forum
-
- 1 follower
- 1 reply
- 11.7k views
Follow these steps to transfer software authorization from one computer to another: 1) Install the PMAC Executive PRO2 Suite software package on the TARGET computer and run it. Once prompted choose to register the software and the software will provide you with a Site Code. (the Site Code will be generated after installing the trial version, downloadable from www.deltatau.com ) 2) Obtain the Site Code from the TARGET computer. 3) Run the PEWIN32PRO2 on the SOURCE computer which already has the license. 4) From the Help menu, Choose “Transfer License” on the SOURCE computer. 5) Enter the Site Code from the TARGET computer that you got in step 2 into the "Site Code" …
Last reply by terrydeltasigmacorp.com, -
- 1 follower
- 2 replies
- 1.2k views
Hi everyone! The CK3M is my device and I have purchased PDK. Now I try to program in C# to connect with CK3M for host computer. I have copied the file(.pmc or .plc) to /var/ftp/usrflash and I can find it with PUTTY. but I cant copies files from flash into RAM. For example, I typed code "system gpascii -i{/path/File.plc}" in IDE Terminal, and Message below, system gpascii -i/var/ftp/usrflash/Temp/prog1.pmc /var/ftp/usrflash/Temp/prog1.pmc:0:2: error #20: ILLEGAL CMD: /*For more information see notes.txt in the Documentation folder */ furthermore, I try to get manual or help of gpascii command in Linux but failed. Could you give me some document on it? PS:I have purchas…
Last reply by Eric Hotchkiss, -
- 1 follower
- 1 reply
- 737 views
Hello, can some body give me the firmware which is Turbo1 V1.947 (11-01-10). Thanks
Last reply by Eric Hotchkiss, -
- 1 follower
- 1 reply
- 957 views
I had the 3A0-PPCOMM-35X and mail to support@deltatau.com with the S/N of my products and Site Code of my PC. But up to now, I haven't received the messag. How could I got the Software License?
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 2.4k views
We want to use Power Pmac controller with ARM CPU.Can anyone kindly suggest us the power pmac IDE version required for the same ?? Also EC engineer has not been found during installation procedure .How can one obtain EC Engineer through any other source ??
Last reply by Eric Hotchkiss, -
- 1 reply
- 2.3k views
Hi All! Tell me please. I correctly understand the next question. if the axes are integrated into a coordinate system, they perform fully synchronized movements. That is, when the motion parameters of one axis change (external influence), the motion parameters of the other axes in the coordinate system will be adjusted so that the coordinate system moves as close as possible to the calculated trajectory ?? That is, an external impact on any axis will cause a correction of the movement of the other axes? Regards!
Last reply by curtwilson, -
- 1 follower
- 1 reply
- 5.3k views
Dear Sina we are using a lot of turbo pmac ultralite and now old baldor macro drive are obsolete. so we have to retrofit our machine. since we want to keep working with PMAC, we need your support. can we convert turbo pmac ultralite into analog by attaching any accessory card to it. please confirm regards rajkumar attri
Last reply by Gregs, -
- 2 followers
- 2 replies
- 9.6k views
We have used PMAC macros in one of our projects, but we were using PEWIN32Pro to download the CFG to the card each time we made a change. Recently I converted a different project to use macros, but we have developed an application for automatically downloading these CFGs to the cards. Apparently the PCOMM32 driver does not have the capability to parse the macros when using the API download functionality. As I see it, my two options are: 1) Create a macro parser in my downloading application and handle parsing and translating the macros myself, or 2) Acquire the Delta Tau parser utility and distribute it with the installer Can someone point me to a link to the Delta Ta…
Last reply by iannicholson, -
- 1 reply
- 5.1k views
I'd like to measure the time between PowerPMAC received the commmand from the Host PC and Motion Program running starting. I think the Motion Progrram start timming could measure by using Program Running Bit, but I'm not sure about how to measure PowerPMAC receive command timing. If I could check the resister of the PowerPMAC Communication task running bit, Could you tell me how to check it?
Last reply by Clopedandle, -
- 0 replies
- 4.4k views
Hi, Just started using the PPMAC and encountered some errors when running the forward/inverse kinematic subroutines. The forward routine seems to be working, but when I add the file inverse.kin in the project I encounter buffer related errors (closed, in use, etc). The same error shows up as early as the compiler finds open inverse (1). I want to know where exactly this error comes from in my project. Is it something I did not define in the forward kinematics routine? Below is my code for the forward kinematics routine. Am I setting KinAxisUsed correctly? My machine has 5 axes. Thanks! csglobal CtsperMm1; csglobal CtsperMm2; csglobal CtsperMm3; csgloba…
Last reply by johann, -
- 1 follower
- 3 replies
- 6.4k views
We just upgraded from a Turbo Umac 5C0 cpu card to a 5C3 card (memory upgrade only). I have updated all the memory locations for the modbus and all machine functions appear to be working correctly. Upon start-up of PEWin32Pro I get a warning that says the following: "Due to Modbus activity, CommThread will not be started at this time. Unsolicited messages will not be captured properly" This goes away if I put in the 5C0 card again. I am probably missing a setting that I don't know about.
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 5.9k views
Hello, I need help to setup a modbus Geobrick. The Geobrick (master) communicates with a safety PLC (slave) The Modbus protocol says to communicate, you must configure (on the master ) the IP address, the slave number and the register number + function code (3 for Read Holding Registers or 16 for Write Multiple Registers) At PEWIN32, I do not see how to configure the slave number and register number. Can someone explain me? I see, you need to configure the "Modbus reference #", but what data should I put (N° slave + starting adresss?? Unit identifier ?)? When I use a program like "Modbus Doctor", I can read the desired value (see screenshot below). tha…
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 11.2k views
When installing the PCOMM32 Library or executables that use it on Windows 7, you will run into the problem of not being able to insert new PMAC devices in the Select Devices dialog. This is true of all of the programs in the 4.3.2.0 version of the software, and in prior versions, as well. The easiest workaround that will not have your local sysadmin yelling at you is to configure the program to run in Windows XP SP3 compatibility mode. This does not require extended privileges at the system level or running the program as administrator, both of which can be a problem in locations ruled by security freaks as sysadmins. To configure the compatability mode, right click o…
Last reply by steve.milici, -
- 1 follower
- 2 replies
- 11.2k views
This is my first post to the general forum so please excuse me if I'm posting in the wrong thread. I am able to communicate with a UMAC CPU using PEWIN32 Pro2 on a laptop running WIN 8.1 except that the Terminal dialog pops up a generic error message: "Class not registered". Other dialogs such as Position, Watch, etc. work fine. I suspect that this laptop is missing some COM or the likes that is normally expected in a WIN7 OS. Any idea what might be required? Thanks, Scott
Last reply by agman, -
- 3 followers
- 8 replies
- 21.4k views
Will PEWin32 Pro2 Suite load in successfully on a Windows 8 platform? Tim
Last reply by agman, -
- 2 followers
- 1 reply
- 5.9k views
Is there any single document somewhere that lists all the products that have been CE certified and have declarations of CE conformity?
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 6.6k views
Dear Sir in my old cnc's i am using baldor macro drives and i want to replace those drives with GEO GMH152/051 drives, so please post any write up, for geo macro setup with turbo pmac 2 through pewin32 pro. as currently i am in doubt what pwn frequencies i have to set as shown in manual. when i make setup through "geo macro drive manual", i am getting fictious noise in velocity whether motor is in open loop. so please help. regards rajkumar attri
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 6.4k views
Is there a comprehensive list of the end of life for all delta tau products (and what is obsolete)? Specifically I would like to know about Turbo and its last few predecessors.
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 8.6k views
PMAC tuning pro was working correctly earlier. Now, when it tries to download the auto-generated PLC code it generates an error because it puts the string "(null)" on five lines. Here is the contents of C:\Program Files\Delta Tau\PMAC Executive Pro2 Suite\PmacTuningPro2\PositionStepTurbo#3.pmc: ;Position Step Trajectory Program For Turbo (null) (null) (null) (null) (null) M923->* M902->* M922->* M921->* M920->* M919->* M913->* M914->* M923->* M902->X:0,24 M922->X:$10F0,24 M921->X:$10F1,24 M919->X:$6,19 M913->D:$00188 M914->Y:$1c0,2,1 OPEN PLC 31 CLEAR M919=1 M913=M913+P907 M921=M902 WHILE(M902-M921ENDW M913=M913-P907 M922…
Last reply by Sina.Sattari, -
serial cable pinouts
by Guest DavisG- 0 replies
- 7.1k views
For those who need a serial cable ( RS232 or RS485 ) connection to a pmac board of any age I have attached the pdf containing all serial cable pinouts. Note: If using the old 26 pin connector the easiest thing is to use a press on ribbon cable DB25 connector to a press on ribbon cable IDC26 connector. Cut wire 26 at the DB25. Then use a standard DB25 to DB9 adapter. If using the 10 pin connector the easiest thing is to use a press on ribbon cable DB9 connector to a press on ribbon cable IDC10 connector. Cut wire 10 at the DB9. for search compatibility - RS-232 or RS-485 serial cable.pdf
-
- 2 followers
- 4 replies
- 13.1k views
our PLC ACC-68M is broken, some outputs are damaged, we want to replace with new one. Any one can teach me how to replace ACC-68M and initialize the unit? Thanks lot
Last reply by Sina.Sattari, -
- 1 follower
- 0 replies
- 4.9k views
Testing one-two-three.
Last reply by steve.milici, -
- 1 follower
- 2 replies
- 9.2k views
LS, Searching for information on this forum I received the following error: "[i]Sorry, but you can only perform one search every 60 seconds. Please wait another 50 seconds before attempting to search again.[/i]" Question: why is there a limit in how fast one is allowed to use this great source of information? If I get no answers to a search, I rephrase and try again... normally. regards, Meindert
Last reply by meindert.norg, -
- 1 follower
- 0 replies
- 5.2k views
While the application is running right click the tray icon and hit ‘Transfer License’. It will bring up a dialog with instructions……
Last reply by Unit101, -
- 0 replies
- 5.8k views
Hi, According to the Quick Reference, we can define up to 255 ASCII caracters as a MACRO definition, but looks like it is 32 caracters maximum in reality. Am I something wrong? Please let me know if there is any way to expand this limitation. Thanks, Junji
Last reply by Junji,