teapotbxy Posted March 30 Share Posted March 30 Hello everyone, I need some help with ACC65E recognization. I'm using a Power PMAC 465 CPU with 4 ACC24E3s and an ACC65E on a 3U UMAC rack. The thing is, ACC 65E cannot be recognized in the IDE, while 4 ACC24E3 are successfully shown. I have switched different slots, but nothing happens. According to manual, I have set ALL SW1 switches to ON, and then finished the declaration of the pointer as the manual said. PTR Input1->ACC65E[0].DataReg[0].0.1; PTR Input2->ACC65E[0].DataReg[0].1.1; etc. and PTR Output1->ACC65E[0].DataReg[3].0.1; PTR Output2->ACC65E[0].DataReg[3].1.1; With this fonfiguration, I got "stdin:7:26: Struct Write Gate Part Number Error" when output was written to 1, and "input1=nan" when reading input1. Is there anything I can do to fix this? Thanks a lot! Quote Link to comment Share on other sites More sharing options...
steve.milici Posted April 3 Share Posted April 3 This would most probably indicate the card is not functioning and will require repair. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted April 3 Share Posted April 3 Make sure jumper E1 is set 1-2. Quote Link to comment Share on other sites More sharing options...
teapotbxy Posted April 6 Author Share Posted April 6 Thank you Steve, The card has been sent for repair. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.