PMAC Technology FAQ
Frequently Asked Questions about PMAC Technology.
40 topics in this forum
-
- 1 follower
- 1 reply
- 11.9k views
When installing the PCOMM32 Library or executables that use it on Windows 7, you will run into the problem of not being able to insert new PMAC devices in the Select Devices dialog. This is true of all of the programs in the 4.3.2.0 version of the software, and in prior versions, as well. The easiest workaround that will not have your local sysadmin yelling at you is to configure the program to run in Windows XP SP3 compatibility mode. This does not require extended privileges at the system level or running the program as administrator, both of which can be a problem in locations ruled by security freaks as sysadmins. To configure the compatability mode, right click o…
Last reply by steve.milici, -
- 2 replies
- 12k views
This is my first post to the general forum so please excuse me if I'm posting in the wrong thread. I am able to communicate with a UMAC CPU using PEWIN32 Pro2 on a laptop running WIN 8.1 except that the Terminal dialog pops up a generic error message: "Class not registered". Other dialogs such as Position, Watch, etc. work fine. I suspect that this laptop is missing some COM or the likes that is normally expected in a WIN7 OS. Any idea what might be required? Thanks, Scott
Last reply by agman, -
- 1 follower
- 8 replies
- 22.3k views
Will PEWin32 Pro2 Suite load in successfully on a Windows 8 platform? Tim
Last reply by agman, -
- 1 follower
- 1 reply
- 6.4k views
Is there any single document somewhere that lists all the products that have been CE certified and have declarations of CE conformity?
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 7.1k views
Dear Sir in my old cnc's i am using baldor macro drives and i want to replace those drives with GEO GMH152/051 drives, so please post any write up, for geo macro setup with turbo pmac 2 through pewin32 pro. as currently i am in doubt what pwn frequencies i have to set as shown in manual. when i make setup through "geo macro drive manual", i am getting fictious noise in velocity whether motor is in open loop. so please help. regards rajkumar attri
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 6.9k views
Is there a comprehensive list of the end of life for all delta tau products (and what is obsolete)? Specifically I would like to know about Turbo and its last few predecessors.
Last reply by steve.milici, -
- 1 follower
- 1 reply
- 9.1k views
PMAC tuning pro was working correctly earlier. Now, when it tries to download the auto-generated PLC code it generates an error because it puts the string "(null)" on five lines. Here is the contents of C:\Program Files\Delta Tau\PMAC Executive Pro2 Suite\PmacTuningPro2\PositionStepTurbo#3.pmc: ;Position Step Trajectory Program For Turbo (null) (null) (null) (null) (null) M923->* M902->* M922->* M921->* M920->* M919->* M913->* M914->* M923->* M902->X:0,24 M922->X:$10F0,24 M921->X:$10F1,24 M919->X:$6,19 M913->D:$00188 M914->Y:$1c0,2,1 OPEN PLC 31 CLEAR M919=1 M913=M913+P907 M921=M902 WHILE(M902-M921ENDW M913=M913-P907 M922…
Last reply by Sina.Sattari, -
serial cable pinouts
by Guest DavisG- 0 replies
- 7.7k views
For those who need a serial cable ( RS232 or RS485 ) connection to a pmac board of any age I have attached the pdf containing all serial cable pinouts. Note: If using the old 26 pin connector the easiest thing is to use a press on ribbon cable DB25 connector to a press on ribbon cable IDC26 connector. Cut wire 26 at the DB25. Then use a standard DB25 to DB9 adapter. If using the 10 pin connector the easiest thing is to use a press on ribbon cable DB9 connector to a press on ribbon cable IDC10 connector. Cut wire 10 at the DB9. for search compatibility - RS-232 or RS-485 serial cable.pdf
-
- 2 followers
- 4 replies
- 13.5k views
our PLC ACC-68M is broken, some outputs are damaged, we want to replace with new one. Any one can teach me how to replace ACC-68M and initialize the unit? Thanks lot
Last reply by Sina.Sattari, -
- 1 follower
- 0 replies
- 5.3k views
Testing one-two-three.
Last reply by steve.milici, -
- 1 follower
- 2 replies
- 9.7k views
LS, Searching for information on this forum I received the following error: "[i]Sorry, but you can only perform one search every 60 seconds. Please wait another 50 seconds before attempting to search again.[/i]" Question: why is there a limit in how fast one is allowed to use this great source of information? If I get no answers to a search, I rephrase and try again... normally. regards, Meindert
Last reply by meindert.norg, -
- 1 follower
- 0 replies
- 5.8k views
While the application is running right click the tray icon and hit ‘Transfer License’. It will bring up a dialog with instructions……
Last reply by Unit101, -
- 0 replies
- 6.2k views
Hi, According to the Quick Reference, we can define up to 255 ASCII caracters as a MACRO definition, but looks like it is 32 caracters maximum in reality. Am I something wrong? Please let me know if there is any way to expand this limitation. Thanks, Junji
Last reply by Junji, -
- 1 follower
- 1 reply
- 9.8k views
Usually I use Pewin32 under an administrator account. How to use it under a user (no administrator) account with XP-sp3, with Vista ?
Last reply by Omron Forums Support, -
- 2 followers
- 1 reply
- 7.2k views
TEst to see if I can post and send a attachement ...[hr] Any ideas why I can't seem to load a attachment with post ??
Last reply by Sina.Sattari,