Jmurphy
-
Posts
2 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by Jmurphy
-
-
I've recently been tasked with starting the transition between Turbo PMAC to Power PMAC. As we progress, I need a short-term solution for machine support and am attempting to connect via a TCP socket on port 1025 per the manual. I saw in another thread a post about and ethernet communications manual, but the link has since decayed. I understand this is obsolete and support is limited.
I have established the socket connection but am having issues getting the drive to respond to the "0x40 0xB0 #4J+" commands.
I'm assuming it should be "00110000 01111000 00110100 00110000 00100000 00110000 01111000 01000010 00110000 00100000 00100011 00110100 01001010 00101011" but cannot find a working example.
Power Brick Ethernet/IP
in Power PMAC
Posted
I have the Ethernet/IP Activated on the Brick but and getting an IOI Syntax Error when trying to read the output array.
Data type: DINT 4byte Output[25]
Data type: DINT 4byte Input[25]
I have and Explicit UDP CIP Data Table Read
Connection Path: 2,IP Address
Source Element: Eip.Connection[0].Output.Idata[0]
Number of Elements: 25
Destination Element: EIP_Output DINT[25]
I also tried with a Generic Ethernet Module
Input and Output Instances as Listed on the EIP Tab
Output 25x32 bit
Input 25x32 bit
Configuration 1 0x8bit
Is there and AOP or an EDS for this hardware to directly connect to a Rockwell Automation PLC or will this have to be handled in a standalone application or would it be better to create a Logix Socket for communication?
Thank you