Yes, these motors have a brake. As you approach full speed the noise is much more noticeable. Also when moving the motors by hand with the geobrick disconnected there seems to be more noticeable trouble turning the shaft every 90 degrees or so. The motor is a four poles, 220V AC induction servo with Endat 2.1 Absolute encoders. Through tuning I have reduced the noise and it will follow perfectly a step move,sin wave move, and trapezoidal move. I am going back to the motor manufacture again with the noise it is making and see if I can get more from them or see if the brake could be causing, the noise. Thanks for the help.