erikj
-
Posts
34 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by erikj
-
-
I am trying to set up a Kollmorgen AKM11C motor with a PPMAC/ACC-24E3/U042. I can do it manually, but when I try to use Tools->MotorSetup I get the following error: 12/8/2010 :3:17 PM - 192.168.0.200, Module - Global Clock : Master Gate Not Found 12/8/2010 :3:17 PM - 192.168.0.200, Module - Global Clock : Can Not CalculateServoPeriod! No MasterGate All my PMAC components are new and I am running with the latest firmware (1.2.1.5). Any help is appreciated. Thanks, Erik
-
[quote='bradp' pid='894' dateline='1291417061'] [b]Question:[/b] I am having trouble getting the PPMAC IDE to run. I am getting the following pop-up message when I start the IDE (see below). Any help you can give me is appreciated. I am using Win7 Pro running in a VMWare Virtual Machine on a Linux workstation. All my other Win7 apps run fine. Any help you can give me is appreciated. I am basically stuck until I can get this to work. [b]Solution:[/b] Unfortunately in Windows Vista and Windows 7 you must run the IDE as an administrator. If the customer didn't run the IDE as an administrator for the first time, they have to uninstall the IDE and reinstall it since there are special procedures that get executed only on initial run. So here are the things I would suggest for the user to follow: 1. Run the IDE as an administrator (right click on the IDE icon and select run as an administrator, or go to properties and under compatibility tab, select run as an administrator) 2. If step 1 didn't help, Uninstall the IDE and restart the computer. 3. Reinstall the IDE. 4. Before running the IDE for the first time after reinstall, right click on the IDE icon and select properties. 5. Under compatibility tab select "Run as an Administrator" and click OK. 6. Run the IDE. [/quote] What you describe above is exactly the problem. The initial execution of the IDE was not as admin. I removed and reinstalled, started as admin, and everything runs fine.
-
[quote='erikj' pid='909' dateline='1291667818'] [quote='erikj' pid='908' dateline='1291667354'] [quote='erikj' pid='907' dateline='1291666287'] [quote='bradp' pid='905' dateline='1291665677'] From the linux side without the win7 vmware running try to SSH to the ppmac. Let me know what happens [/quote] [erikj@laplace erikj]$ ssh 192.168.0.200 ssh: connect to host 192.168.0.200 port 22: Connection refused [/quote] Hi Brad, just to be sure it isn't the cable (although ping shouldn't work if it is), I tried using a different network cable. This particular cable is straight through, not a crossover. Evidently one of the two sides or both can auto negotiate and account for the cable. In the end I get the same results: I can ping but I cannot telnet or ssh into the PPMAC. Thanks, Erik [/quote] Is there a way to use USB or RS-232 to get a console connection into the PPMAC so we can see what is going on? [/quote] Hi Brad, I just power cycled the PPMAC and now I can get in just fine. Sorry for the bother -- I should have tried that before calling for help. Thanks for your replies. Erik
-
[quote='erikj' pid='908' dateline='1291667354'] [quote='erikj' pid='907' dateline='1291666287'] [quote='bradp' pid='905' dateline='1291665677'] From the linux side without the win7 vmware running try to SSH to the ppmac. Let me know what happens [/quote] [erikj@laplace erikj]$ ssh 192.168.0.200 ssh: connect to host 192.168.0.200 port 22: Connection refused [/quote] Hi Brad, just to be sure it isn't the cable (although ping shouldn't work if it is), I tried using a different network cable. This particular cable is straight through, not a crossover. Evidently one of the two sides or both can auto negotiate and account for the cable. In the end I get the same results: I can ping but I cannot telnet or ssh into the PPMAC. Thanks, Erik [/quote] Is there a way to use USB or RS-232 to get a console connection into the PPMAC so we can see what is going on?
-
[quote='erikj' pid='907' dateline='1291666287'] [quote='bradp' pid='905' dateline='1291665677'] From the linux side without the win7 vmware running try to SSH to the ppmac. Let me know what happens [/quote] [erikj@laplace erikj]$ ssh 192.168.0.200 ssh: connect to host 192.168.0.200 port 22: Connection refused [/quote] Hi Brad, just to be sure it isn't the cable (although ping shouldn't work if it is), I tried using a different network cable. This particular cable is straight through, not a crossover. Evidently one of the two sides or both can auto negotiate and account for the cable. In the end I get the same results: I can ping but I cannot telnet or ssh into the PPMAC. Thanks, Erik
-
[quote='bradp' pid='905' dateline='1291665677'] From the linux side without the win7 vmware running try to SSH to the ppmac. Let me know what happens [/quote] [erikj@laplace erikj]$ ssh 192.168.0.200 ssh: connect to host 192.168.0.200 port 22: Connection refused
-
[quote='bradp' pid='903' dateline='1291662066'] Have you ever been able to Telnet to this PPmac? Are you on a network or a point to point connection? [/quote] Yes, we originally used it a few weeks ago from a laptop running win7. Both Atul and Sina helped us get the PPMAC IDE running and we were able to talk to it and eventually tune a motor. I am now using a different host CPU. a Linux box. I am using VMWare to run Win7 and have the PPMAC IDE running on that. I can ping from both Linux and Win7 to reach the board, but cannot telnet in. The connection is point-to-point using a cat 5 crossover cable. The IP address of the network interface on the host side is 192.168.0.100.
-
Hi, I am unable to telnet into my PPMAC host -- I get a connection refused error. PPMAC board is set to default IP address of 192.168.0.200. I can reach it via ping, so I am confused as to what is wrong. Please see output below. I am running under linux from the command line. The IP addtress of the linux host is 192.168.0.100 and I have a direct connection using a crossover cable to the PPMAC board. The connection refused response comes back immediately, there is no delay. Any help you can give me is appreciated. Thanks, Erik [erikj@laplace erikj]$ ping -c 5 192.168.0.200 PING 192.168.0.200 (192.168.0.200) 56(84) bytes of data. 64 bytes from 192.168.0.200: icmp_seq=1 ttl=64 time=0.074 ms 64 bytes from 192.168.0.200: icmp_seq=2 ttl=64 time=0.087 ms 64 bytes from 192.168.0.200: icmp_seq=3 ttl=64 time=0.069 ms 64 bytes from 192.168.0.200: icmp_seq=4 ttl=64 time=0.050 ms 64 bytes from 192.168.0.200: icmp_seq=5 ttl=64 time=0.080 ms --- 192.168.0.200 ping statistics --- 5 packets transmitted, 5 received, 0% packet loss, time 4000ms rtt min/avg/max/mdev = 0.050/0.072/0.087/0.012 ms [erikj@laplace erikj]$ telnet 192.168.0.200 Trying 192.168.0.200... telnet: connect to address 192.168.0.200: Connection refused telnet: Unable to connect to remote host: Connection refused [erikj@laplace erikj]$
Error: No Master Gate
in Power PMAC
Posted