The linear motor is Tecnotion UC06 with 0.1um/cts Grating ruler,our current motor setup configue is below:
Is our configure right? The nominalrpm and maxrpm parameters seem to be no use,so they may can be remove from IDE?If they do not need,can you remove them from IDE when motor type is line motor.
First I wired the motor U,V,W in good order,then I change the order into random.
When I changed the U,V,W in random order,it still phase Ok,but will it run normal?
If I run IDE motor setup again,will it be good again without change wire?